Hello,
I am working on a project with the C5535 and I read on the datasheet that I can get an analogue output signal via the GPIO pins, but I do not know how. Could someone help me with the code that I would have to write in order to get a square pulse from a pin on the C5535, in fact, it doesn't have to be by the GPIO pins necessarily, any pin or terminal I could get a signal from is fine. The purpose is to work with that analogue signal on a PIC afterwards.
I'd appreciate your help.
Sincerely, Osmar.