Other Parts Discussed in Thread: DM385
Tool/software: Linux
Hi Sir,
The original design was working fine.For some reason we need to change the NAND flash.But when we changed to new NAND flash.the system can not boot up.Please help to check it.
1.the informations of new NAND flash are
Toshiba TC58NVG0S3HYA00 (128M + 8 bit)
page size is 2176 bytes
block size is (128+8k)bytes
Do I need to modify the information in the driver?where do I modify it?
2.The error message are be below.
U-Boot 2010.06 (Jul 20 2017 - 16:40:41) DM385_IPNC_3.50.00
NAND device: Manufacturer ID: 0x98, Chip ID: 0xf1 (Toshiba NAND 128MiB 3,3V 8-bit)
Data (writethrough) Cache is ON
Loading from NAND 128MiB 3,3V 8-bit, offset 0x280000
Image Name: Linux-2.6.37_DM385_3.50.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1763520 Bytes = 1.7 MiB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Linux-2.6.37_DM385_3.50.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1763520 Bytes = 1.7 MiB
Load Address: 80008000
Entry Point: 80008000
OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Trying to install type control for IRQ375
Trying to set irq flags for IRQ375
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_late_init: Voltage driver support not added
INIT: version 2.86 booting
Kernel panic - not syncing: Attempted to kill init!
Backtrace:
[<c0041f70>] (dump_backtrace+0x0/0x110) from [<c027317c>] (dump_stack+0x18/0x1c)
r6:c6826000 r5:00007f00 r4:c0391998 r3:60000013
[<c0273164>] (dump_stack+0x0/0x1c) from [<c02731dc>] (panic+0x5c/0x178)
[<c0273180>] (panic+0x0/0x178) from [<c0068858>] (do_exit+0x68/0x5d0)
r3:c036fedc r2:c6829f18 r1:00000001 r0:c030e131
r7:000000f8
[<c00687f0>] (do_exit+0x0/0x5d0) from [<c0069070>] (do_group_exit+0x84/0xb4)
r7:000000f8
[<c0068fec>] (do_group_exit+0x0/0xb4) from [<c00690b8>] (sys_exit_group+0x18/0x20)
r4:00000005 r3:0000007f
[<c00690a0>] (sys_exit_group+0x0/0x20) from [<c003e3c0>] (ret_fast_syscall+0x0/0x30)
Best Regards,
Byron