Part Number: AM3354
Hi,
I have a question about AM335x IBIS Model.
On my customer's board NAND Flash are connected to AM3354 GPMC.
And they want to simutate GPMC - NAND Flash signals by using IBIS model.
In IBIS of AM335x, Model Selector for GPMC signals are "Selector_14" or "Selector_15".
There are many model_xxx in each Model Selector, and we don't know which model should be used.
So, which model_xxx in each Selector(14 & 15) should be used for
simulating GPMC - NAND Flash signals?
best regards,
g.f.