Part Number: AM3352
Other Parts Discussed in Thread: SYSCONFIG
Tool/software: Linux
Hi,
we are planning to create a Linux Embedded Device that uses EHRPWM to generate a PWM output while the AM3352 CPU is in Linux standby mode (not Deepsleep0).
(see
)
I noticed that the PWM subsystem is inside the peripheral power domain
Is it possible to use the PWM outputs while the CPU is in sleep mode and does the linux suspend code possibly support this?
We are still using Processor SDK 1.0 (kernel 3.14.y) but will possibly upgrade to the latest version soon.
Regards,
Bastian Schmitz