TMS320C6457
Fixed-Point Digital Signal Processor
Silicon Errata
Literature Number: SPRZ293A
November 2009
Silicon Revisions 1.0, 1.1, 1.2, 1.3, 1.4
In the silicon errata guide, it states that the processor revisions affected are 1.4, but the individual items only state 1.3. Is this stating that the revision affected is 1.4 only because it was fixed in this release? Are there no advisories for Silicon Revision 1.4? For example, port0 affects revision 1.4, but the advisory says it affects 1.3.
Can you provide guidance/clarification on how to read this?
Page 12
Silicon Updates www.ti.com
Silicon Revisions 1.0, 1.1, 1.2, 1.3, 1.4 Submit Documentation Feedback
Advisory 3 SRIO Port0 Reset Issue
Revision(s) Affected: 1.3, 1.2, 1.1, 1.0
Page 8
See table 3, page 8 where it states that this applies to Revision 1.4.
Thanks
Will