Part Number: TDA3
Hello,
the OSC0 is connected with a 20 MHz crystal and I need 25 MHz at CLKOUT1 output to drive a UB960 serializer. Currently I found only PLL divider for the CLKOUT. Is there an other way to get 25 MHz?
In another possible case, if I use 25 MHz at OSC1, I get 25 MHz at CLKOUT1. So it could be the best solution. Are there some disadvantages according to VSDK or other thinks? Why is the OSC1 on the EVM connected to a 22.5792 MHz crystal?
Best regards,
Milan