Other Parts Discussed in Thread: TLV320ADC3101
Dear all:
We are using TLV320ADC23B with DM365 and using the DVSDK_2_10_00_17 for development.
When running the encode demo in dvsdk, we found an error :
root@DVS365:/opt/dm365# ./encode -s test.g711
Encode demo started.
Error: Failed to create speech device
The audio codec in EVMDM365 is TLV320ADC3101, so does that difference matter? If so,
do I need to change the audio driver in Linux?