Part Number: TDA3
Hello,
I am working on a custom board with TDA3 and UB960 deserializer, connected to the OV10640 sensor via UB953 serializer. The framerate of the sensor is asynchron to the display framerate and is drifting apart, so buffer overflow or underflow occurs periodically after few seconds.
Now I want synchronize sensor and display with external sensor triggering. I am considering that the display is the master, so VSYNC or DSS-IRQ-event could be a source for the sensor trigger signal.
Is it possible to use the DSS-IRQ-event to drive e.g. a timer with GPIO output to generate a narrow positive trigger puls?
Is there another solution to synchronize sensor and display?
Best Regards,
Milan