Tool/software: Linux
Hi,
What is the maximum permissible CPU load for both the cores of AM5728?
What is the maximum allowed temperature for AM5728 and thermal cutoff limits?
Please suggest means to measure CPU load of AM5728 with LInux SDK loaded.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hi,
What is the maximum permissible CPU load for both the cores of AM5728?
What is the maximum allowed temperature for AM5728 and thermal cutoff limits?
Please suggest means to measure CPU load of AM5728 with LInux SDK loaded.
Hi Marka,
You can check the CPU load by top Linux command. The maximum load is 1.00 which refers to 100% CPU load.
You can find information about allowed working temperature for AM5728 in the datasheet at:
www.ti.com/.../am5728.pdf
but in general Operating junction temperature range is 0 to 90 °C for commercial and -40 to 105 °C for extended devices.
BR
Tsvetolin Shulev