Dear all:
Recently I have compiled NK.bin use based on the latest OMAP3530 WINCE BSP version BSP_WINCE_ARM_A8-1.00.00.11, but there is no serial output messages of NK.bin and display also no signal when I booted omap3530 from SD card . Some messages before jump to NK.bin are as follows:
BL_IMAGE_TYPE_BIN Download file information: ----------------------------------------------------------- [0]: Address=0x80002000 Length=0x0170b394 Save=0x80002000 ----------------------------------------------------------- Download file type: 1 ...................................................................................................................................................................................rom_offset=0x0. ..ImageStart = 0x80002000, ImageLength = 0x170B394, LaunchAddr = 0x800114E0 Completed file(s): ------------------------------------------------------------------------------- [0]: Address=0x80002000 Length=0x170B394 Name="" Target=RAM ROMHDR at Address 80002044h Launch Windows CE image by jumping to 0x800114e0... "Launch Windows CE image by jumping to 0x800114e0..." is the last output messages . Can everyone tell me the reason? Thanks in Advance for your support!