Part Number: TDA3XEVM
Other Parts Discussed in Thread: FFTLIB
Hello,
I am using CCS 6.1.1 with Vision SDK 2.8.0.0. I have the following RTSC components installed:
(1) Code Generation Tools Version 7.4.2
(2) XDC 3.32.00.06
(3) BIOS 6.45.00.20
(4) EDMA3 2.12.0.0
(5) XDAIS 7.24.00.04
I am trying to optimize FFT and IFFT computations in my current project. These computations are running on a single C66x DSP core. But I am not able to understand how to integrate the kernels from the C66x FFTLIB into my source code. I tried to perform a standalone build of two kernels from the library, referring to the FFTLIB user manual for kernel build steps. I am receiving multiple errors related to missing RTSC components, and I am not able to understand how to resolve these with my current development environment.
Is it even possible to use the C66x FFTLIB for TDA3x device? If 'yes', how can I compile and link the FFTLIB kernels with my current development environment? Do I absolutely need to install the C66x DSPLIB to build the C66x FFTLIB?
Thank you in advance.