Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
hi
I have been using image from beaglebone.org for my beaglebone black. But now I want to try stuff like building the u-boot and kernel so I try the TI SDK.
My question is: I have download the SDK from "http://software-dl.ti.com/processor-sdk-linux-rt/esd/AM335X/latest/index_FDS.html" . I directly start using the "create_sdcard.sh" to format the SD card and install the pre-built image, when I put it to the BBB, it boots. However, the display shows nothing and it is black showing text "please wait.." and nothing happens then.
I google a bit and said that I need to run "setup.sh" to further configure BBB. I wonder when should I run this script? From here "http://elinux.org/Beagleboard:3.2_SDK_On_BeagleBone_Black
pre-built image. Then connect to BBB with router and usb and run the "setup.sh".