Part Number: DM385
Hi Everyone,
I'm currently working on a custom design based around a DM385. Our software originated from a development board developed by nSketch, our PSP package is "psp_04_04_00_02" if that helps.
The DevKit contained 512MB of ram, I believe it's address mapping is like this:
256MB at address 0x80000000 - 0x90000000
256MB at address 0xB0000000 - 0xC0000000
Our custom board is using 1GB total, two 512MB chips. I believe it's address mapping is like this:
512MB at address 0x80000000 - 0xA0000000
512MB at address 0xA0000000 - 0xC0000000
As you can see, it's basically filling in the 512MB gap in the original mapping.
Our kernel boot argument is:
"console=ttyO0,115200n8 rootwait=1 rw ubi.mtd=7,2048 rootfstype=ubifs root=ubi0:rootfs init=/sbin/init mem=92M vram=8M notifyk.vpssm3_sva=0xBFD00000 ip=off eth=$(ethaddr) cmemk.phys_start=0x85C00000 cmemk.phys_end=0x8AE00000 cmemk.allowOverlap=1 earlyprintk"
mem=92M - I take this to mean 92M@0x80000000
cmemk.phys_start=0x85C00000 cmemk.phys_end=0x8AE00000 cmemk.allowOverlap=1 - CMEM region from 0x85C00000 to 0x8AE00000
The .bld file our project uses (mcfw/src_bios6/cfg/ti810x/config_512M.bld) gives the following memory map that seems to match up:
/* first 256MB */ var LINUX_SIZE = 92*MB; var CMEM_SIZE = 82*MB; var SR1_SIZE = 50*MB; var VIDEO_M3_CODE_SIZE = 512*KB; var VIDEO_M3_DATA_SIZE = 512*KB; var DSS_M3_CODE_SIZE = 4*MB; var DSS_M3_DATA_SIZE = 26*MB; var DSP_CODE_SIZE = 512*KB; var DSP_DATA_SIZE = 512*KB; /* second 256MB */ var TILER_SIZE = 16*MB; /* Reducing this to fix Vid Frame Alloc failures. Need to fix */ /* MUST be aligned on 128MB boundary */ var SR2_FRAME_BUFFER_SIZE = 217*MB; // set over 128M if tiler is enabled var SR0_SIZE = 16*MB; var VIDEO_M3_EXCEPTION_CTX_SIZE = 128*KB; var VPSS_M3_EXCEPTION_CTX_SIZE = 128*KB; var HDVPSS_DESC_SIZE = 2*MB; var HDVPSS_SHARED_SIZE = 2*MB - 256*KB; var NOTIFY_SHARED_SIZE = 2*MB; var REMOTE_DEBUG_SIZE = 1*MB;
What I would like to do is give the 512MB from 0x90000000 - 0xB0000000 to Linux so my user applications can use it. If I can get away with it, I'd like to leave all other allocations in the memory map untouched to minimize changes to the system.
Here are the experiments I've done so far to try to get an understanding of the situation. It should be noted that I have not yet modified the .bld file to account for the entire 1GB of RAM, so this might be my issue.
1. In uboot, I've ran mtest over the range of 0xA0000000 - 0xC0000000 (skipping first 256MB, didn't want to blow up uboot and I wasn't sure how much memory uboot was using). mtest did not detect any issues after a 5 or 6 iterations with different test data. Not a thorough test, but I figured it was a good start.
2. Just add the following to the bootargs "mem=512M@0x90000000", so for example:
"console=ttyO0,115200n8 rootwait=1 rw ubi.mtd=7,2048 rootfstype=ubifs root=ubi0:rootfs init=/sbin/init mem=92M mem=512M@0x90000000 vram=8M notifyk.vpssm3_sva=0xBFD00000 ip=off eth=$(ethaddr) cmemk.phys_start=0x85C00000 cmemk.phys_end=0x8AE00000 cmemk.allowOverlap=1 earlyprintk"
The system boots normally to command prompt. The kernel initialization prints indicate it has the additional memory accounted for:
Memory: 92MB 502MB 1MB = 595MB total Memory: 597996k/597996k available, 20500k reserved, 0K highmem
And /proc/meminfo also indicates the memory is there:
MemTotal: 598200 kB
However, when I start loading the MCFW firmware, I have issues:
root@DM385_CBB:~/video# ./remote_debug_client.out 0xbff00000 & root@DM385_CBB:~/video# [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000 [m3video] Remote Debug Shared Memory @ 0xbff05020 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040 root@DM385_CBB:~/video# insmod syslink.ko SysLink version : 2.21.02.10 SysLink module created on Date:Jul 25 2017 Time:12:58:38 root@DM385_CBB:~/video# ./fw_load.out startup VPSS-M3 carbb_rdk_fw_m3vpss.xem3 [host] Attached to slave procId 1. vmap allocation for size 21929984 failed: use vmalloc=<size> to increase size. Unable to handle kernel NULL pointer dereference at virtual address 00000000 pgd = ee718000 [00000000] *pgd=aea20031, *pte=00000000, *ppte=00000000 Internal error: Oops: 817 [#1] last sysfs file: Modules linked in: syslink bat_irq g_ether ti81xx nop_usb_xceiv cppi41dma musb_hdrc CPU: 0 Not tainted (2.6.37_DM385_CBB_0.80.00 #2) PC is at __memzero+0x24/0x80 LR is at 0x0 pc : [<c0194604>] lr : [<00000000>] psr: 20000013 sp : eea57d24 ip : 00000000 fp : 0000000a r10: 00000005 r9 : f1de8000 r8 : 06a85000 r7 : f1d79000 r6 : 00000000 r5 : 014e8b48 r4 : eea57db8 r3 : 00000000 r2 : 00000000 r1 : 014e8b08 r0 : 00000000 Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user Control: 10c5387d Table: ae718019 DAC: 00000015 Process fw_load.out (pid: 173, stack limit = 0xeea562e8) Stack: (0xeea57d24 to 0xeea58000) 7d20: bf04a850 8e500000 003a429a 003a429a 00000001 bf0e4948 00000001 7d40: 00000001 00000000 00000000 8e500000 8e500000 bf058094 014e8b48 00000000 7d60: 00000001 bf0e4948 003a429a 8e500000 00000070 f1dd8000 00000001 f1de8000 7d80: f1e4e0c0 f1deb000 f1de8000 00000005 0000000a bf04e400 00000002 bf04cdcc 7da0: ef3bfb80 eecdf280 00000000 00000000 00000002 f1dd801c f1de8000 f1e5d000 7dc0: f7400000 00000001 003a4480 00000000 00000002 00000020 f1deb000 f1deb000 7de0: 00000000 03046000 f1d79000 f1d73000 00000000 00000000 00000000 bf0e4948 7e00: beeefaf4 bf04a274 f1de5000 00000000 00000000 00000000 eea57e34 f1de8000 7e20: ee402080 f1d73000 00000000 f1de5000 00000000 bf0e4948 00000000 bf045c1c 7e40: 00000000 eea57f00 00000000 00000000 bf0e4948 f1d85000 00000000 00000000 7e60: f1de5000 eea57f00 00000000 bf046b48 00000000 eea57f00 00000000 00000000 7e80: beeefa90 00000000 c020e0a2 f1de5000 00000000 eea56000 00000000 bf048ed8 7ea0: 00000000 eea57f00 000006e0 c01c9a50 ef13c400 c01cb7e4 00000002 0000000a 7ec0: ef19e000 000006ba ef19e000 c01d0da0 a0000013 ee9be380 00000000 c01c9a3c 7ee0: c01c9c08 40361000 f1d85000 beeefda8 00000019 00000000 00000000 00000000 7f00: 00000000 ef19a9f0 eea56000 00000000 eecddc80 00000008 beeefa90 00000008 7f20: 00000000 c00c407c ee918000 ee918000 00000025 c01b2440 ee99fbc0 c01b4bd8 7f40: 0000009d 2d4cae03 00000001 ee9be380 40dd7000 eea57f80 00000000 00000025 7f60: eea56000 00000000 ee9be380 eeb0a380 beeefa90 c020e0a2 00000008 00000000 7f80: eea56000 c00c413c 00000008 00000001 0001f1c4 00000000 beeefa90 00000036 7fa0: c0040604 c0040480 0001f1c4 00000000 00000008 c020e0a2 beeefa90 00000008 7fc0: 0001f1c4 00000000 beeefa90 00000036 00000000 00000000 4011b000 beeefaf4 7fe0: c020e0a2 beeefa78 00013840 402f81cc 20000010 00000008 afefe021 afefe421 Code: e52de004 e1a0c002 e1a0e002 e2511040 (a8a0500c) ---[ end trace d633e997e115e877 ]---
3. I get the same issue if I reduce this new linux memory section to 256MB (0x90000000 - 0xA0000000)
4. The closest I've gotten to getting something to work is to move the CMEM location to 0x90000000 - 0xA0000000 (256MB) and allocate from it. For some reason, the mcfw firmware didn't blow up with this configuration. Unfortunately, due to the structure of our application, we cannot use CMEM allocations.
So my question is, what is the right way of going about increasing the memory available to Linux?
Thanks!