Other Parts Discussed in Thread: TVP5158, TVP7002
Hi all,
I am using the following code to create capture instance
/*Capture Link params*/
CaptureLink_CreateParams_Init(&capturePrm);
//capturePrm.numVipInst = 2;
capturePrm.numVipInst = 1;
capturePrm.outQueParams[0].nextLink = gVdisModuleContext.displayId[VDIS_DEV_HDMI];
capturePrm.tilerEnable = FALSE;
capturePrm.vipInst[0].vipInstId = SYSTEM_CAPTURE_INST_VIP0_PORTA; //PORTA:24bit data, PORTB:8bit data
pCaptureInstPrm = &capturePrm.vipInst[0];
//pCaptureInstPrm->standard = SYSTEM_STD_1080P_60;
pCaptureInstPrm->standard = SYSTEM_STD_1080I_60;//SYSTEM_STD_VGA_60;
pCaptureInstPrm->numOutput = 1;
pCaptureOutPrm = &pCaptureInstPrm->outParams[0];
pCaptureOutPrm->dataFormat = SYSTEM_DF_YUV422SP_UV;
pCaptureOutPrm->scEnable = FALSE;
pCaptureOutPrm->scOutWidth = 1920;
pCaptureOutPrm->scOutHeight = 1080;
pCaptureOutPrm->outQueId = 0;
while creating the link the following error has been encountered
" Front Left: Capture 80 [67%] [40.00dB] [on]nks_m3vpss/capture/captureLink_drv.c: pInst->captureVipHandle != NULL : failed !!!:
I am using ipnc rdk 3.8 and my input is through VGA cable connected from cpu and output is hdmi display. I am using DM388EVM.
Please suggest the solutions.
Thanks
Kailash