This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM4378: How do I keep the RTC Timer while the power is off in AM4378?

Part Number: AM4378

Tool/software: Linux

Hi all.

I built boards based on the AM4378 EVM board.
And I got into some problems.

First, the power supply of 1.8V is continuously maintained through the PMIC in the VDDS_RTC of the AM4378.

On Linux, we stored the time information in the RTC using the date and hwclock -w commands.

However, the RTC is not retained after the main power of the AM4378 is turned off.
(1.8V is maintained in VDDS_RTC.)

For what?

Below is a circuit diagram of the crystal part.
It is oscillating even when main power is off.

Please Help me..

I want the RTC clock to be maintained by 1.8v of VDDS_RTC even when the power is off.