Other Parts Discussed in Thread: DRA742
We are using DRA742, BSP version (7.04.00.03), QSPI flash:STMicro N25Q128. We are doing long-term test in our custom board(system will do some test, then power-off, power-on, and repeat the tests). Sometimes QSPI flash probe fail at boot phase, so i can't access flash at kernel through "mtd_debug" command.
Because temperature will vary during the test, so, could it possible the fail reason is because temperature?
Right now, fail happend at CPU-temperature 32 and 95 degree(not always, system can also probe flash success at lower than 32 or higher than 95 temperature). I alreday check the SPEC. of flash, it should work fine at -40 ~ 105 degree.
When flash probe fail, i can see "ti-qspi 4b300000.qspi: write timed out" and "spi_master spi32766: failed to transfer one message from queue" these message.
Here is the log for probe success at boot phase=>
U-Boot SPL 2014.07 (Aug 17 2017 - 14:00:21)
DRA752-GP ES2.0
ti_i2c_eeprom_init failed 1
===EMIF-(1) Interface Setting===
Use emif1_ddr3_532_mhz_1csti_i2c_eeprom_init failed 1
U-Boot 2014.07 (Aug 17 2017 - 14:00:21)
CPU : DRA752-GP ES2.0
Board: DRA74x EVM REV <NULL>
I2C: ready
DRAM: 256 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Using default environment
serial# not set, setting...
SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
SCSI: Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw
Hit any key to stop autoboot: 0
@ADAPTER@
XXXX SD clock downto 20000000
switch to partitions #0, OK
mmc0 is current device
XXXX SD clock downto 20000000
SD/MMC found on device 0
reading uEnv.txt
221 bytes read in 3 ms (71.3 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc0 ...
3875176 bytes read in 437 ms (8.5 MiB/s)
109113 bytes read in 33 ms (3.2 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x3b2168 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8e6fd000, end 8e71aa38 ... OK
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 3.14.63 (jonathan_hsu@tpedmcbm03) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #1 SMP PREEMPT Wed Aug 23 20:33:06 CST 2017
CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=10c5387d
CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
Machine model: TI DRA742
cma: CMA: reserved 64 MiB at 8a400000
Memory policy: Data cache writealloc
DRA752 ES2.0
PERCPU: Embedded 8 pages/cpu @cfc98000 s8384 r8192 d16192 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64768
Kernel command line: console=ttyO3,115200n8 elevator=noop root=PARTUUID=d9567eff-02 rw rootwait earlyprintk fixrtc omapdrm.num_crtc=2 consoleblank=0 cma=64M rootfstype=ext4 snd.slots_reserved=1,1
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 184796K/261120K available (5207K kernel code, 354K rwdata, 1932K rodata, 272K init, 240K bss, 76324K reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0xc0008000 - 0xc0700fb4 (7140 kB)
.init : 0xc0701000 - 0xc07450c0 ( 273 kB)
.data : 0xc0746000 - 0xc079ea70 ( 355 kB)
.bss : 0xc079ea7c - 0xc07dacd4 ( 241 kB)
Preemptible hierarchical RCU implementation.
NR_IRQS:16 nr_irqs:16 16
@@@set sys_clkin1 as abe_dpll_mux's parent
OMAP clockevent source: timer1 at 32786 Hz
sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 65536000000000ns
OMAP clocksource: 32k_counter at 32768 Hz
Architected cp15 timer(s) running at 6.14MHz (virt).
sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 2794592043008ns
Switching to timer-based delay loop
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
/cpus/cpu@1 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x8051bd68 - 0x8051bdc0
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated (24.59 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
omap_hwmod: l3_main_2 using broken dt data from ocp
omap_hwmod: tptc0 using broken dt data from edma-controller
omap_hwmod: tptc1 using broken dt data from edma-controller
omap_hwmod: dcan1: _wait_target_disable failed
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
syscon 4a002000.tisysconcore: regmap [mem 0x4a002000-0x4a0026cf] registered
syscon 4a002e00.tisyscon: regmap [mem 0x4a002e00-0x4a002e7b] registered
OMAP GPIO hardware version 0.1
irq: no irq domain found for /ocp/pinmux@4a003400 !
omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/pinmux@4a003400/nand_flash_x16, deferring probe
platform 50000000.gpmc: Driver omap-gpmc requests probe deferral
No ATAGs?
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
OMAP DMA hardware revision 0.0
bio: create slab <bio-0> at 0
edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver
evm_3v3_sd: 3300 mV
reg-fixed-voltage fixedregulator-sd: Failed to find supply vin
reg-fixed-voltage fixedregulator-sd: Failed to register regulator: -517
platform fixedregulator-sd: Driver reg-fixed-voltage requests probe deferral
evm_3v3_sw: 3300 mV
reg-fixed-voltage fixedregulator-evm_3v3_sw: Failed to find supply vin
reg-fixed-voltage fixedregulator-evm_3v3_sw: Failed to register regulator: -517
platform fixedregulator-evm_3v3_sw: Driver reg-fixed-voltage requests probe deferral
aic_dvdd: 1800 mV
reg-fixed-voltage fixedregulator-aic_dvdd: Failed to find supply vin
reg-fixed-voltage fixedregulator-aic_dvdd: Failed to register regulator: -517
platform fixedregulator-aic_dvdd: Driver reg-fixed-voltage requests probe deferral
vmmcwl_fixed: 1800 mV
vtt_fixed: 1350 mV
reg-fixed-voltage fixedregulator-vtt: Failed to find supply vin
reg-fixed-voltage fixedregulator-vtt: Failed to register regulator: -517
platform fixedregulator-vtt: Driver reg-fixed-voltage requests probe deferral
i2c-core: driver [palmas] using legacy suspend method
i2c-core: driver [palmas] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
palmas 0-0058: IRQ missing: skipping irq request
palmas 0-0058: Muxing GPIO a, PWM 0, LED 0
prom_parse: Bad cell count for /ocp/i2c@48070000/tps659038@58
SMPS12: at 1070 mV
SMPS3: at 1350 mV
smps45: 850 <--> 1500 mV at 990 mV
smps6: 850 <--> 1500 mV at 1080 mV
smps7: 850 <--> 1500 mV at 1060 mV
smps8: 850 <--> 1500 mV at 1010 mV
smps9: 1800 mV
ldo1: 1800 <--> 3300 mV at 3300 mV
ldo2: 3300 mV
ldo3: 1800 mV
LDO4: no parameters
LDO5: no parameters
LDO6: no parameters
LDO7: no parameters
LDO8: no parameters
ldo9: 1050 mV
ldoln: 1800 mV
ldousb: 3300 mV
REGEN1: no parameters
regen2: no parameters
sysen1: no parameters
sysen2: no parameters
pcf857x: probe of 0-0020 failed with error -121
pcf857x: probe of 0-0027 failed with error -121
pcf857x: probe of 0-0021 failed with error -121
omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
omap_i2c 48072000.i2c: controller timed out
pcf857x: probe of 1-0026 failed with error -110
omap_i2c 48072000.i2c: bus 1 rev0.12 at 400 kHz
omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
pcf857x: probe of 3-0021 failed with error -121
omap_i2c 4807a000.i2c: bus 3 rev0.12 at 400 kHz
omap_i2c 4807c000.i2c: bus 4 rev0.12 at 400 kHz
Linux video capture interface: v2.00
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource arch_sys_counter
NET: Registered protocol family 2
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 2048 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP: reno registered
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
hw perfevents: enabled with ARMv7 Cortex-A15 PMU driver, 7 counters available
futex hash table entries: 512 (order: 3, 32768 bytes)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
msgmni has been set to 488
alg: No test for stdrng (krng)
NET: Registered protocol family 38
io scheduler noop registered (default)
io scheduler deadline registered
io scheduler cfq registered
pinctrl-single 4a003400.pinmux: 281 pins at pa fc003400 size 1124
pbias_mmc_omap5: 1800 <--> 3000 mV at 3000 mV
abb_mpu: 1100 <--> 1210 mV
abb_ivahd: 1060 <--> 1250 mV
abb_dspeve: 1060 <--> 1250 mV
abb_gpu: 1060 <--> 1280 mV
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
4806a000.serial: ttyO0 at MMIO 0x4806a000 (irq = 299, base_baud = 3000000) is a OMAP UART0
omap_uart 4806c000.serial: no wakeirq for uart0
4806c000.serial: ttyO1 at MMIO 0x4806c000 (irq = 300, base_baud = 3000000) is a OMAP UART1
omap_uart 48020000.serial: no wakeirq for uart0
48020000.serial: ttyO2 at MMIO 0x48020000 (irq = 301, base_baud = 3000000) is a OMAP UART2
omap_uart 4806e000.serial: no wakeirq for uart0
4806e000.serial: ttyO3 at MMIO 0x4806e000 (irq = 302, base_baud = 3000000) is a OMAP UART3
console [ttyO3] enabled
omap_uart 48422000.serial: no wakeirq for uart0
48422000.serial: ttyO7 at MMIO 0x48422000 (irq = 303, base_baud = 3000000) is a OMAP UART7
omap_uart 48424000.serial: no wakeirq for uart0
48424000.serial: ttyO8 at MMIO 0x48424000 (irq = 304, base_baud = 3000000) is a OMAP UART8
omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
brd: module loaded
loop: module loaded
(stk) :sysfs entries created
(stk) : debugfs entries created
(hci_tty): inside hci_tty_init
(hci_tty): allocated 251, 0
mtdoops: mtd device (mtddev=name/number) must be supplied
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver smsc95xx
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-omap: OMAP-EHCI Host Controller driver
usbcore: registered new interface driver cdc_wdm
usbcore: registered new interface driver usb-storage
mousedev: PS/2 mouse device common for all mice
omap_rtc 48838000.rtcss: rtc core: registered 48838000.rtcss as rtc0
i2c /dev entries driver
Driver for 1-wire Dallas network protocol.
coproc iva_coproc: probe
Adding alias for supply vdd,iva_coproc -> vdd,4a0025cc.voltdm
Adding alias for supply vbb,iva_coproc -> vbb,4a0025cc.voltdm
coproc iva_coproc: coproc_probe result=0
coproc dsp_coproc: probe
Adding alias for supply vdd,dsp_coproc -> vdd,4a0025e0.voltdm
Adding alias for supply vbb,dsp_coproc -> vbb,4a0025e0.voltdm
coproc dsp_coproc: coproc_probe result=0
omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
omap_hsmmc 4809c000.mmc: unable to get vmmc regulator -517
platform 4809c000.mmc: Driver omap_hsmmc requests probe deferral
omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
alg: skcipher: setkey failed on test 5 for ecb-des-omap: flags=100
alg: skcipher-ddst: setkey failed on test 5 for ecb-des-omap: flags=100
alg: skcipher-ddst: setkey failed on test 5 for ecb-des-omap: flags=100
omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
omap-sham 4b101000.sham: initialization failed.
omap-sham: probe of 4b101000.sham failed with error -22
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
[mcaspdrv_init]
mcaspdrv_init called
============[davinci_mcasp_probe]==============
====>pm_runtime_forbid
davinci-mcasp 48464000.mcasp: DAI is shared
=========> [davinci_mcasp_probe] mem->start = [48464000] <==
=========> [davinci_mcasp_probe] mcasp->base = [D091C000] <==
============[davinci_mcasp_probe]==============
====>pm_runtime_forbid
davinci-mcasp 48468000.mcasp: DAI is shared
=========> [davinci_mcasp_probe] mem->start = [48468000] <==
=========> [davinci_mcasp_probe] mcasp->base = [D0934000] <==
=====[McASP3]====
=====[mcasp][CF1C3E10]=====
=====[mcasp->base][D0934000]=====
============[davinci_mcasp_probe]==============
====>pm_runtime_forbid
davinci-mcasp 48474000.mcasp: DAI is shared
=========> [davinci_mcasp_probe] mem->start = [48474000] <==
=========> [davinci_mcasp_probe] mcasp->base = [D0938000] <==
============[davinci_mcasp_probe]==============
====>pm_runtime_forbid
davinci-mcasp 48460000.mcasp: DAI is shared
=========> [davinci_mcasp_probe] mem->start = [48460000] <==
=========> [davinci_mcasp_probe] mcasp->base = [D093C000] <==
=====[McASP1]====
=====[mcasp][CF1C3A10]=====
=====[mcasp->base][D093C000]=====
oprofile: using timer interrupt.
TCP: cubic registered
Initializing XFRM netlink socket
NET: Registered protocol family 17
NET: Registered protocol family 15
Key type dns_resolver registered
Adding ali
0x000000020000-0x000000040000 : "NAND.SPL.backup1"
0x000000040000-0x000000060000 : "NAND.SPL.backup2"
0x000000060000-0x000000080000 : "NAND.SPL.backup3"
0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os"
0x0000000c0000-0x0000001c0000 : "NAND.u-boot"
0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env"
0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1"
0x000000200000-0x000000a00000 : "NAND.kernel"
0x000000a00000-0x000010000000 : "NAND.file-system"
evm_3v3_sd: 3300 mV
evm_3v3_sd: supplied by sysen1
evm_3v3_sw: 3300 mV
evm_3v3_sw: supplied by sysen1
aic_dvdd: 1800 mV
aic_dvdd: supplied by evm_3v3_sw
vtt_fixed: 1350 mV
vtt_fixed: supplied by sysen2
pbias_mmc_omap5: unsupportable voltage range: 3300000-3000000uV
pbias_mmc_omap5: unsupportable voltage range: 3300000-3000000uV
pbias_mmc_omap5: unsupportable voltage range: 3300000-3000000uV
pbias_mmc_omap5: unsupportable voltage range: 3300000-3000000uV
pbias_mmc_omap5: unsupportable voltage range: 3300000-3000000uV
pbias_mmc_omap5: unsupportable voltage range: 3300000-3000000uV
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
mmc0: host does not support reading read-only switch. assuming write-enable.
XXXX SD clock downto 20000000
mmc0: new high speed SDHC card at address 59b4
davinci_mdio 48485000.mdio: davinci mdio revision 1.6
davinci_mdio 48485000.mdio: detected phy mask fffffffa
libphy: 48485000.mdio: probed
davinci_mdio 48485000.mdio: phy[0]: device 48485000.mdio:00, driver unknown
davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver unknown
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
cpsw 48484000.ethernet: Detected MACID = c8:fd:19:b7:5d:60
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
cpsw 48484000.ethernet: cpsw: Detected MACID = c8:fd:19:b7:5d:61
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
omap_rtc 48838000.rtcss: setting system clock to 2000-01-01 00:00:01 UTC (946684801)
mmcblk0: mmc0:59b4 SDC 7.26 GiB
ALSA device list:
mmcblk0: p1 p2
No soundcards found.
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
EXT4-fs (mmcblk0p2): recovery complete
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 272K (c0701000 - c0745000)
INIT: version 2.88 booting
Starting udev
udevd[1042]: starting version 182
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
CAN device driver interface
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
c_can_platform 4ae3c000.can: c_can_platform device registered (regs=fce3c000, irq=346)
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
m25p80 spi32766.0: n25q128a13 (16384 Kbytes)
10 ofpart partitions found on MTD device spi32766.0
Creating 10 MTD partitions on "spi32766.0":
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
0x000000000000-0x000000040000 : "QSPI.MLO"
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
0x000000040000-0x000000140000 : "QSPI.u-boot"
0x000000140000-0x0000001c0000 : "QSPI.DRA7-evm.dtb"
0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
0x0000001e0000-0x0000009e0000 : "QSPI.uImage"
0x0000009e0000-0x000002000000 : "QSPI.IPU-exe"
mtd: partition "QSPI.IPU-exe" extends beyond the end of device "spi32766.0" -- size truncated to 0x620000
0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
0x0000001e0000-0x0000009e0000 : "QSPI.kernel"
0x0000009e0000-0x000002000000 : "QSPI.file-system"
mtd: partition "QSPI.file-system" extends beyond the end of device "spi32766.0" -- size truncated to 0x620000
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
omapdrm_pvr: Unknown symbol omap_drm_unregister_mapper (err 0)
omapdrm_pvr: Unknown symbol omap_gem_set_sync_object (err 0)
omapdrm_pvr: Unknown symbol omap_gem_priv (err 0)
omapdrm_pvr: Unknown symbol omap_drm_file_priv (err 0)
omapdrm_pvr: Unknown symbol omap_gem_put_paddr (err 0)
omapdrm_pvr: Unknown symbol drm_gem_handle_delete (err 0)
omapdrm_pvr: Unknown symbol omap_gem_op_async (err 0)
omapdrm_pvr: Unknown symbol drm_gem_object_lookup (err 0)
omapdrm_pvr: Unknown symbol omap_gem_tiled_stride (err 0)
omapdrm_pvr: Unknown symbol omap_gem_new_ext (err 0)
omapdrm_pvr: Unknown symbol drm_gem_object_free (err 0)
omapdrm_pvr: Unknown symbol drm_gem_vm_close (err 0)
omapdrm_pvr: Unknown symbol omap_drm_register_plugin (err 0)
omapdrm_pvr: Unknown symbol drm_gem_handle_create (err 0)
omapdrm_pvr: Unknown symbol omap_drm_register_mapper (err 0)
omapdrm_pvr: Unknown symbol omap_gem_get_paddr (err 0)
omapdrm_pvr: Unknown symbol omap_gem_tiled_size (err 0)
omapdrm_pvr: Unknown symbol omap_drm_unregister_plugin (err 0)
omapdrm_pvr: Unknown symbol omap_gem_get_pages (err 0)
omapdrm_pvr: Unknown symbol omap_gem_put_pages (err 0)
omapdrm_pvr: Unknown symbol drm_mmap (err 0)
omapdrm_pvr: Unknown symbol omap_gem_op_update (err 0)
omapdrm_pvr: Unknown symbol omap_gem_set_priv (err 0)
omapdrm_pvr: Unknown symbol omap_drm_file_set_priv (err 0)
omapdrm_pvr: Unknown symbol omap_gem_flags (err 0)
omapdrm_pvr: Unknown symbol omap_gem_mmap_offset (err 0)
udevd[1318]: failed to execute '/etc/udev/scripts/mount.sh' '/etc/udev/scripts/mount.sh': No such file or directomapdrm_pvr: Unknown symbol omap_drm_unregister_mapper (err 0)
ory
omapdrm_pvr: Unknown symbol omap_gem_set_sync_object (err 0)
omapdrm_pvr: Unknown symbol omap_gem_priv (err 0)
omapdrm_pvr: Unknown symbol omap_drm_file_priv (err 0)
omapdrm_pvr: Unknown symbol omap_gem_put_paddr (err 0)
omapdrm_pvr: Unknown symbol drm_gem_handle_delete (err 0)
omapdrm_pvr: Unknown symbol omap_gem_op_async (err 0)
omapdrm_pvr: Unknown symbol drm_gem_object_lookup (err 0)
omapdrm_pvr: Unknown symbol omap_gem_tiled_stride (err 0)
omapdrm_pvr: Unknown symbol omap_gem_new_ext (err 0)
omapdrm_pvr: Unknown symbol drm_gem_object_free (err 0)
omapdrm_pvr: Unknown symbol drm_gem_vm_close (err 0)
omapdrm_pvr: Unknown symbol omap_drm_register_plugin (err 0)
omapdrm_pvr: Unknown symbol drm_gem_handle_create (err 0)
omapdrm_pvr: Unknown symbol omap_drm_register_mapper (err 0)
omapdrm_pvr: Unknown symbol omap_gem_get_paddr (err 0)
omapdrm_pvr: Unknown symbol omap_gem_tiled_size (err 0)
omapdrm_pvr: Unknown symbol omap_drm_unregister_plugin (err 0)
omapdrm_pvr: Unknown symbol omap_gem_get_pages (err 0)
omapdrm_pvr: Unknown symbol omap_gem_put_pages (err 0)
omapdrm_pvr: Unknown symbol drm_mmap (err 0)
omapdrm_pvr: Unknown symbol omap_gem_op_update (err 0)
omapdrm_pvr: Unknown symbol omap_gem_set_priv (err 0)
omapdrm_pvr: Unknown symbol omap_drm_file_set_priv (err 0)
omapdrm_pvr: Unknown symbol omap_gem_flags (err 0)
omapdrm_pvr: Unknown symbol omap_gem_mmap_offset (err 0)
udevd[1320]: failed to execute '/etc/udev/scripts/mount.sh' '/etc/udev/scripts/mount.sh': No such file or directory
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
xhci-hcd xhci-hcd.0.auto: irq 422, io mem 0x48890000
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: xHCI Host Controller
usb usb1: Manufacturer: Linux 3.14.63 xhci-hcd
usb usb1: SerialNumber: xhci-hcd.0.auto
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: xHCI Host Controller
usb usb2: Manufacturer: Linux 3.14.63 xhci-hcd
usb usb2: SerialNumber: xhci-hcd.0.auto
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
xhci-hcd xhci-hcd.1.auto: irq 423, io mem 0x488d0000
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
usb usb3: New USB device found, idVendor=1d6b, idProduct=0002
usb usb3: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb3: Product: xHCI Host Controller
usb usb3: Manufacturer: Linux 3.14.63 xhci-hcd
usb usb3: SerialNumber: xhci-hcd.1.auto
hub 3-0:1.0: USB hub found
hub 3-0:1.0: 1 port detected
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4
usb usb4: New USB device found, idVendor=1d6b, idProduct=0003
usb usb4: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb4: Product: xHCI Host Controller
usb usb4: Manufacturer: Linux 3.14.63 xhci-hcd
usb usb4: SerialNumber: xhci-hcd.1.auto
hub 4-0:1.0: USB hub found
hub 4-0:1.0: 1 port detected
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
random: nonblocking pool is initialized
EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
ALSA: Restoring mixer settings...
/usr/sbin/alsactl: load_state:1729: No soundcards found...
Thu Mar 24 18:36:00 UTC 2016
[INFO] VERSION: R0.2.0.0015
[INFO] memory test PASS
[SYS ] paring option: token=3, option=(null)
[INFO] R3 init
INIT: Entering runlevel: 5
Configuring network interfaces... net eth0: initializing cpsw version 1.15 (0)
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
net eth0: phy found : id is : 0x221560
udhcpc (v1.22.1) started
Sending discover...
libphy: 48485000.mdio:00 - Link is Up - 100/Full
Sending discover...
Sending discover...
No lease, forking to background
done.
Starting system message bus: dbus.
UIM SYSFS Node Found at /sys/./devices/kim/install
Starting uim-sysfs daemon.
uim:@ main
uim:install = /sys/./devices/kim/install
uim:dev_name = /sys/./devices/kim/dev_name
uim:baud_rate = /sys/./devices/kim/baud_rate
uim:flow_cntrl = /sys/./devices/kim/flow_cntrl
uim:begin polling...
Starting telnet daemon.
Starting tiipclad daemon
GateMP support enabled on host
Opened log file: lad.txt
numProcessors = 5 id = 0 baseId = 0
Spawned daemon: /usr/bin/lad_dra7xx
.
Starting rpcbind daemon...rpcbind: cannot create socket for udp6
rpcbind: cannot create socket for tcp6
done.
creating NFS state directory: done
starting statd: done
NFS daemon support not enabled in kernel
Starting syslogd/klogd: done
Starting thttpd.
Enabling thermal zones...
Stopping Bootlog daemon: bootlogd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dra7xx-evm ttyO3
Arago 2013.10 dra7xx-evm ttyO3
dra7xx-evm login: root (automatic login)
root@dra7xx-evm:~#
Here is the log for probe fail at boot phase=>
U-Boot SPL 2014.07 (Aug 17 2017 - 14:00:21)
DRA752-GP ES2.0
ti_i2c_eeprom_init failed 1
===EMIF-(1) Interface Setting===
Use emif1_ddr3_532_mhz_1csti_i2c_eeprom_init failed 1
U-Boot 2014.07 (Aug 17 2017 - 14:00:21)
CPU : DRA752-GP ES2.0
Board: DRA74x EVM REV <NULL>
I2C: ready
DRAM: 256 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Using default environment
serial# not set, setting...
SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
SCSI: Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw
Hit any key to stop autoboot: 0
@ADAPTER@
XXXX SD clock downto 20000000
switch to partitions #0, OK
mmc0 is current device
XXXX SD clock downto 20000000
SD/MMC found on device 0
reading uEnv.txt
221 bytes read in 3 ms (71.3 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc0 ...
3875176 bytes read in 438 ms (8.4 MiB/s)
109113 bytes read in 34 ms (3.1 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x3b2168 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8e6fd000, end 8e71aa38 ... OK
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 3.14.63 (jonathan_hsu@tpedmcbm03) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #1 SMP PREEMPT Wed Aug 23 20:33:06 CST 2017
CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=10c5387d
CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
Machine model: TI DRA742
cma: CMA: reserved 64 MiB at 8a400000
Memory policy: Data cache writealloc
DRA752 ES2.0
PERCPU: Embedded 8 pages/cpu @cfc98000 s8384 r8192 d16192 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64768
Kernel command line: console=ttyO3,115200n8 elevator=noop root=PARTUUID=d9567eff-02 rw rootwait earlyprintk fixrtc omapdrm.num_crtc=2 consoleblank=0 cma=64M rootfstype=ext4 snd.slots_reserved=1,1
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 184796K/261120K available (5207K kernel code, 354K rwdata, 1932K rodata, 272K init, 240K bss, 76324K reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0xc0008000 - 0xc0700fb4 (7140 kB)
.init : 0xc0701000 - 0xc07450c0 ( 273 kB)
.data : 0xc0746000 - 0xc079ea70 ( 355 kB)
.bss : 0xc079ea7c - 0xc07dacd4 ( 241 kB)
Preemptible hierarchical RCU implementation.
NR_IRQS:16 nr_irqs:16 16
@@@set sys_clkin1 as abe_dpll_mux's parent
OMAP clockevent source: timer1 at 32786 Hz
sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 65536000000000ns
OMAP clocksource: 32k_counter at 32768 Hz
Architected cp15 timer(s) running at 6.14MHz (virt).
sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 2794592043008ns
Switching to timer-based delay loop
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
/cpus/cpu@1 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x8051bd68 - 0x8051bdc0
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated (24.59 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
omap_hwmod: l3_main_2 using broken dt data from ocp
omap_hwmod: tptc0 using broken dt data from edma-controller
omap_hwmod: tptc1 using broken dt data from edma-controller
omap_hwmod: dcan1: _wait_target_disable failed
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
syscon 4a002000.tisysconcore: regmap [mem 0x4a002000-0x4a0026cf] registered
syscon 4a002e00.tisyscon: regmap [mem 0x4a002e00-0x4a002e7b] registered
OMAP GPIO hardware version 0.1
irq: no irq domain found for /ocp/pinmux@4a003400 !
omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/pinmux@4a003400/nand_flash_x16, deferring probe
platform 50000000.gpmc: Driver omap-gpmc requests probe deferral
No ATAGs?
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
OMAP DMA hardware revision 0.0
bio: create slab <bio-0> at 0
edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver
evm_3v3_sd: 3300 mV
reg-fixed-voltage fixedregulator-sd: Failed to find supply vin
reg-fixed-voltage fixedregulator-sd: Failed to register regulator: -517
platform fixedregulator-sd: Driver reg-fixed-voltage requests probe deferral
evm_3v3_sw: 3300 mV
reg-fixed-voltage fixedregulator-evm_3v3_sw: Failed to find supply vin
reg-fixed-voltage fixedregulator-evm_3v3_sw: Failed to register regulator: -517
platform fixedregulator-evm_3v3_sw: Driver reg-fixed-voltage requests probe deferral
aic_dvdd: 1800 mV
reg-fixed-voltage fixedregulator-aic_dvdd: Failed to find supply vin
reg-fixed-voltage fixedregulator-aic_dvdd: Failed to register regulator: -517
platform fixedregulator-aic_dvdd: Driver reg-fixed-voltage requests probe deferral
vmmcwl_fixed: 1800 mV
vtt_fixed: 1350 mV
reg-fixed-voltage fixedregulator-vtt: Failed to find supply vin
reg-fixed-voltage fixedregulator-vtt: Failed to register regulator: -517
platform fixedregulator-vtt: Driver reg-fixed-voltage requests probe deferral
i2c-core: driver [palmas] using legacy suspend method
i2c-core: driver [palmas] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
palmas 0-0058: IRQ missing: skipping irq request
palmas 0-0058: Muxing GPIO a, PWM 0, LED 0
prom_parse: Bad cell count for /ocp/i2c@48070000/tps659038@58
SMPS12: at 1070 mV
SMPS3: at 1350 mV
smps45: 850 <--> 1500 mV at 990 mV
smps6: 850 <--> 1500 mV at 1080 mV
smps7: 850 <--> 1500 mV at 1060 mV
smps8: 850 <--> 1500 mV at 1010 mV
smps9: 1800 mV
ldo1: 1800 <--> 3300 mV at 3300 mV
ldo2: 3300 mV
ldo3: 1800 mV
LDO4: no parameters
LDO5: no parameters
LDO6: no parameters
LDO7: no parameters
LDO8: no parameters
ldo9: 1050 mV
ldoln: 1800 mV
ldousb: 3300 mV
REGEN1: no parameters
regen2: no parameters
sysen1: no parameters
sysen2: no parameters
pcf857x: probe of 0-0020 failed with error -121
pcf857x: probe of 0-0027 failed with error -121
pcf857x: probe of 0-0021 failed with error -121
omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
omap_i2c 48072000.i2c: controller timed out
pcf857x: probe of 1-0026 failed with error -110
omap_i2c 48072000.i2c: bus 1 rev0.12 at 400 kHz
omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
pcf857x: probe of 3-0021 failed with error -121
omap_i2c 4807a000.i2c: bus 3 rev0.12 at 400 kHz
omap_i2c 4807c000.i2c: bus 4 rev0.12 at 400 kHz
Linux video capture interface: v2.00
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource arch_sys_counter
NET: Registered protocol family 2
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 2048 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP: reno registered
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
hw perfevents: enabled with ARMv7 Cortex-A15 PMU driver, 7 counters available
futex hash table entries: 512 (order: 3, 32768 bytes)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
msgmni has been set to 488
alg: No test for stdrng (krng)
NET: Registered protocol family 38
io scheduler noop registered (default)
io scheduler deadline registered
io scheduler cfq registered
pinctrl-single 4a003400.pinmux: 281 pins at pa fc003400 size 1124
pbias_mmc_omap5: 1800 <--> 3000 mV at 3000 mV
abb_mpu: 1100 <--> 1210 mV
abb_ivahd: 1060 <--> 1250 mV
abb_dspeve: 1060 <--> 1250 mV
abb_gpu: 1060 <--> 1280 mV
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
4806a000.serial: ttyO0 at MMIO 0x4806a000 (irq = 299, base_baud = 3000000) is a OMAP UART0
omap_uart 4806c000.serial: no wakeirq for uart0
4806c000.serial: ttyO1 at MMIO 0x4806c000 (irq = 300, base_baud = 3000000) is a OMAP UART1
omap_uart 48020000.serial: no wakeirq for uart0
48020000.serial: ttyO2 at MMIO 0x48020000 (irq = 301, base_baud = 3000000) is a OMAP UART2
omap_uart 4806e000.serial: no wakeirq for uart0
4806e000.serial: ttyO3 at MMIO 0x4806e000 (irq = 302, base_baud = 3000000) is a OMAP UART3
console [ttyO3] enabled
omap_uart 48422000.serial: no wakeirq for uart0
48422000.serial: ttyO7 at MMIO 0x48422000 (irq = 303, base_baud = 3000000) is a OMAP UART7
omap_uart 48424000.serial: no wakeirq for uart0
48424000.serial: ttyO8 at MMIO 0x48424000 (irq = 304, base_baud = 3000000) is a OMAP UART8
omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
brd: module loaded
loop: module loaded
(stk) :sysfs entries created
(stk) : debugfs entries created
(hci_tty): inside hci_tty_init
(hci_tty): allocated 251, 0
mtdoops: mtd device (mtddev=name/number) must be supplied
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver smsc95xx
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-omap: OMAP-EHCI Host Controller driver
usbcore: registered new interface driver cdc_wdm
usbcore: registered new interface driver usb-storage
mousedev: PS/2 mouse device common for all mice
omap_rtc 48838000.rtcss: rtc core: registered 48838000.rtcss as rtc0
i2c /dev entries driver
Driver for 1-wire Dallas network protocol.
coproc iva_coproc: probe
Adding alias for supply vdd,iva_coproc -> vdd,4a0025cc.voltdm
Adding alias for supply vbb,iva_coproc -> vbb,4a0025cc.voltdm
coproc iva_coproc: coproc_probe result=0
coproc dsp_coproc: probe
Adding alias for supply vdd,dsp_coproc -> vdd,4a0025e0.voltdm
Adding alias for supply vbb,dsp_coproc -> vbb,4a0025e0.voltdm
coproc dsp_coproc: coproc_probe result=0
omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
omap_hsmmc 4809c000.mmc: unable to get vmmc regulator -517
platform 4809c000.mmc: Driver omap_hsmmc requests probe deferral
omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
alg: skcipher: setkey failed on test 5 for ecb-des-omap: flags=100
alg: skcipher-ddst: setkey failed on test 5 for ecb-des-omap: flags=100
alg: skcipher-ddst: setkey failed on test 5 for ecb-des-omap: flags=100
omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
omap-sham 4b101000.sham: initialization failed.
omap-sham: probe of 4b101000.sham failed with error -22
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
[mcaspdrv_init]
mcaspdrv_init called
============[davinci_mcasp_probe]==============
====>pm_runtime_forbid
davinci-mcasp 48464000.mcasp: DAI is shared
=========> [davinci_mcasp_probe] mem->start = [48464000] <==
=========> [davinci_mcasp_probe] mcasp->base = [D091C000] <==
============[davinci_mcasp_probe]==============
====>pm_runtime_forbid
davinci-mcasp 48468000.mcasp: DAI is shared
=========> [davinci_mcasp_probe] mem->start = [48468000] <==
=========> [davinci_mcasp_probe] mcasp->base = [D0934000] <==
=====[McASP3]====
=====[mcasp][CF1E8C10]=====
=====[mcasp->base][D0934000]=====
============[davinci_mcasp_probe]==============
====>pm_runtime_forbid
davinci-mcasp 48474000.mcasp: DAI is shared
=========> [davinci_mcasp_probe] mem->start = [48474000] <==
=========> [davinci_mcasp_probe] mcasp->base = [D0938000] <==
============[davinci_mcasp_probe]==============
====>pm_runtime_forbid
davinci-mcasp 48460000.mcasp: DAI is shared
=========> [davinci_mcasp_probe] mem->start = [48460000] <==
=========> [davinci_mcasp_probe] mcasp->base = [D093C000] <==
=====[McASP1]====
=====[mcasp][CF1E8810]=====
=====[mcasp->base][D093C000]=====
oprofile: using timer interrupt.
TCP: cubic registered
Initializing XFRM netlink socket
NET: Registered protocol family 17
NET: Registered protocol family 15
Key type dns_resolver registered
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
Power Management for TI OMAP4+ devices.
ThumbEE CPU extension supported.
Registering SWP/SWPB emulation handler
REGEN1: disabling
vmmcwl_fixed: disabling
regulator-dummy: disabling
omap-gpmc 50000000.gpmc: GPMC revision 6.0
gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xca
nand: Micron NAND 256MiB 3,3V 16-bit
nand: 256MiB, SLC, page size: 2048, OOB size: 64
nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
10 ofpart partitions found on MTD device omap2-nand.0
Creating 10 MTD partitions on "omap2-nand.0":
0x000000000000-0x000010000000 : "NAND.device.0"
0x000000020000-0x000000040000 : "NAND.SPL.backup1"
0x000000040000-0x000000060000 : "NAND.SPL.backup2"
0x000000060000-0x000000080000 : "NAND.SPL.backup3"
0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os"
0x0000000c0000-0x0000001c0000 : "NAND.u-boot"
0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env"
0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1"
0x000000200000-0x000000a00000 : "NAND.kernel"
0x000000a00000-0x000010000000 : "NAND.file-system"
evm_3v3_sd: 3300 mV
evm_3v3_sd: supplied by sysen1
evm_3v3_sw: 3300 mV
evm_3v3_sw: supplied by sysen1
aic_dvdd: 1800 mV
aic_dvdd: supplied by evm_3v3_sw
vtt_fixed: 1350 mV
vtt_fixed: supplied by sysen2
pbias_mmc_omap5: unsupportable voltage range: 3300000-3000000uV
pbias_mmc_omap5: unsupportable voltage range: 3300000-3000000uV
pbias_mmc_omap5: unsupportable voltage range: 3300000-3000000uV
pbias_mmc_omap5: unsupportable voltage range: 3300000-3000000uV
pbias_mmc_omap5: unsupportable voltage range: 3300000-3000000uV
pbias_mmc_omap5: unsupportable voltage range: 3300000-3000000uV
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
mmc0: host does not support reading read-only switch. assuming write-enable.
XXXX SD clock downto 20000000
mmc0: new high speed SDHC card at address 59b4
davinci_mdio 48485000.mdio: davinci mdio revision 1.6
davinci_mdio 48485000.mdio: detected phy mask fffffffa
mmcblk0: mmc0:59b4 SDC 7.26 GiB
libphy: 48485000.mdio: probed
mmcblk0: p1 p2
davinci_mdio 48485000.mdio: phy[0]: device 48485000.mdio:00, driver unknown
davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver unknown
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
cpsw 48484000.ethernet: Detected MACID = c8:fd:19:b7:5d:60
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpsw 48484000.ethernet: cpsw: Detected MACID = c8:fd:19:b7:5d:61
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
omap_rtc 48838000.rtcss: setting system clock to 2000-01-01 00:00:01 UTC (946684801)
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
ALSA device list:
No soundcards found.
EXT4-fs (mmcblk0p2): recovery complete
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 272K (c0701000 - c0745000)
INIT: version 2.88 booting
Starting udev
udevd[1043]: starting version 182
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
CAN device driver interface
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
c_can_platform 4ae3c000.can: c_can_platform device registered (regs=fce3c000, irq=346)
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
omapdrm_pvr: Unknown symbol omap_drm_unregister_mapper (err 0)
omapdrm_pvr: Unknown symbol omap_gem_set_sync_object (err 0)
omapdrm_pvr: Unknown symbol omap_gem_priv (err 0)
omapdrm_pvr: Unknown symbol omap_drm_file_priv (err 0)
omapdrm_pvr: Unknown symbol omap_gem_put_paddr (err 0)
omapdrm_pvr: Unknown symbol drm_gem_handle_delete (err 0)
omapdrm_pvr: Unknown symbol omap_gem_op_async (err 0)
omapdrm_pvr: Unknown symbol drm_gem_object_lookup (err 0)
omapdrm_pvr: Unknown symbol omap_gem_tiled_stride (err 0)
omapdrm_pvr: Unknown symbol omap_gem_new_ext (err 0)
omapdrm_pvr: Unknown symbol drm_gem_object_free (err 0)
omapdrm_pvr: Unknown symbol drm_gem_vm_close (err 0)
omapdrm_pvr: Unknown symbol omap_drm_register_plugin (err 0)
omapdrm_pvr: Unknown symbol drm_gem_handle_create (err 0)
omapdrm_pvr: Unknown symbol omap_drm_register_mapper (err 0)
omapdrm_pvr: Unknown symbol omap_gem_get_paddr (err 0)
omapdrm_pvr: Unknown symbol omap_gem_tiled_size (err 0)
omapdrm_pvr: Unknown symbol omap_drm_unregister_plugin (err 0)
omapdrm_pvr: Unknown symbol omap_gem_get_pages (err 0)
omapdrm_pvr: Unknown symbol omap_gem_put_pages (err 0)
omapdrm_pvr: Unknown symbol drm_mmap (err 0)
omapdrm_pvr: Unknown symbol omap_gem_op_update (err 0)
omapdrm_pvr: Unknown symbol omap_gem_set_priv (err 0)
omapdrm_pvr: Unknown symbol omap_drm_file_set_priv (err 0)
omapdrm_pvr: Unknown symbol omap_gem_flags (err 0)
omapdrm_pvr: Unknown symbol omap_gem_mmap_offset (err 0)
omapdrm_pvr: Unknown symbol omap_drm_unregister_mapper (err 0)
omapdrm_pvr: Unknown symbol omap_gem_set_sync_object (err 0)
omapdrm_pvr: Unknown symbol omap_gem_priv (err 0)
omapdrm_pvr: Unknown symbol omap_drm_file_priv (err 0)
omapdrm_pvr: Unknown symbol omap_gem_put_paddr (err 0)
omapdrm_pvr: Unknown symbol drm_gem_handle_delete (err 0)
omapdrm_pvr: Unknown symbol omap_gem_op_async (err 0)
omapdrm_pvr: Unknown symbol drm_gem_object_lookup (err 0)
omapdrm_pvr: Unknown symbol omap_gem_tiled_stride (err 0)
omapdrm_pvr: Unknown symbol omap_gem_new_ext (err 0)
omapdrm_pvr: Unknown symbol drm_gem_object_free (err 0)
omapdrm_pvr: Unknown symbol drm_gem_vm_close (err 0)
omapdrm_pvr: Unknown symbol omap_drm_register_plugin (err 0)
omapdrm_pvr: Unknown symbol drm_gem_handle_create (err 0)
omapdrm_pvr: Unknown symbol omap_drm_register_mapper (err 0)
omapdrm_pvr: Unknown symbol omap_gem_get_paddr (err 0)
omapdrm_pvr: Unknown symbol omap_gem_tiled_size (err 0)
omapdrm_pvr: Unknown symbol omap_drm_unregister_plugin (err 0)
omapdrm_pvr: Unknown symbol omap_gem_get_pages (err 0)
omapdrm_pvr: Unknown symbol omap_gem_put_pages (err 0)
omapdrm_pvr: Unknown symbol drm_mmap (err 0)
omapdrm_pvr: Unknown symbol omap_gem_op_update (err 0)
omapdrm_pvr: Unknown symbol omap_gem_set_priv (err 0)
omapdrm_pvr: Unknown symbol omap_drm_file_set_priv (err 0)
omapdrm_pvr: Unknown symbol omap_gem_flags (err 0)
omapdrm_pvr: Unknown symbol omap_gem_mmap_offset (err 0)
udevd[1307]: failed to execute '/etc/udev/scripts/mount.sh' '/etc/udev/scripts/mount.sh': No such file or directory
udevd[1308]: failed to execute '/etc/udev/scripts/mount.sh' '/etc/udev/scripts/mount.sh': No such file or directory
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
random: nonblocking pool is initialized
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
xhci-hcd xhci-hcd.0.auto: irq 422, io mem 0x48890000
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: xHCI Host Controller
usb usb1: Manufacturer: Linux 3.14.63 xhci-hcd
usb usb1: SerialNumber: xhci-hcd.0.auto
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: xHCI Host Controller
usb usb2: Manufacturer: Linux 3.14.63 xhci-hcd
usb usb2: SerialNumber: xhci-hcd.0.auto
cpu cpu0: cpu0 clock notifier not ready, retry
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3
xhci-hcd xhci-hcd.1.auto: irq 423, io mem 0x488d0000
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
usb usb3: New USB device found, idVendor=1d6b, idProduct=0002
usb usb3: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb3: Product: xHCI Host Controller
usb usb3: Manufacturer: Linux 3.14.63 xhci-hcd
usb usb3: SerialNumber: xhci-hcd.1.auto
hub 3-0:1.0: USB hub found
hub 3-0:1.0: 1 port detected
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4
usb usb4: New USB device found, idVendor=1d6b, idProduct=0003
usb usb4: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb4: Product: xHCI Host Controller
usb usb4: Manufacturer: Linux 3.14.63 xhci-hcd
usb usb4: SerialNumber: xhci-hcd.1.auto
hub 4-0:1.0: USB hub found
hub 4-0:1.0: 1 port detected
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
ti-qspi 4b300000.qspi: write timed out
spi_master spi32766: failed to transfer one message from queue
[LabVIEW] [2017/09/10 04:03:28][ego --start]
udevd[1043]: worker [1088] timeout, kill it
udevd[1043]: seq 1120 '/devices/44000000.ocp/4b300000.qspi/spi_master/spi32766/spi32766.0' killed
EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
ALSA: Restoring mixer settings...
/usr/sbin/alsactl: load_state:1729: No soundcards found...
Thu Mar 24 18:36:00 UTC 2016
[INFO] VERSION: R0.2.0.0015
[INFO] memory test PASS
[SYS ] paring option: token=3, option=(null)
[INFO] R3 init,
INIT: Entering runlevel: 5
Configuring network interfaces... net eth0: initializing cpsw version 1.15 (0)
Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
omap_voltdm 4a003b20.voltdm: Unable to get vdd regulator:-517
cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
cpu cpu0: cpu0 clock notifier not ready, retry
platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
net eth0: phy found : id is : 0x221560
udhcpc (v1.22.1) started
Sending discover...
[INFO] HOST connected
Sending discover...
libphy: 48485000.mdio:00 - Link is Up - 100/Full
Sending discover...
No lease, forking to background
done.
Starting system message bus: dbus.
UIM SYSFS Node Found at /sys/./devices/kim/install
Starting uim-sysfs daemon.
uim:@ main
uim:install = /sys/./devices/kim/install
uim:dev_name = /sys/./devices/kim/dev_name
uim:baud_rate = /sys/./devices/kim/baud_rate
uim:flow_cntrl = /sys/./devices/kim/flow_cntrl
uim:begin polling...
Starting telnet daemon.
Starting tiipclad daemon
GateMP support enabled on host
Opened log file: lad.txt
numProcessors = 5 id = 0 baseId = 0
Spawned daemon: /usr/bin/lad_dra7xx
.
Starting rpcbind daemon...rpcbind: cannot create socket for udp6
rpcbind: cannot create socket for tcp6
done.
creating NFS state directory: done
starting statd: done
NFS daemon support not enabled in kernel
Starting syslogd/klogd: done
Starting thttpd.
Enabling thermal zones...
Stopping Bootlog daemon: bootlogd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dra7xx-evm ttyO3
Arago 2013.10 dra7xx-evm ttyO3
dra7xx-evm login: root (automatic login)
root@dra7xx-evm:~#
Regards,
Shawn