Other Parts Discussed in Thread: OMAP-L138
I have been running into a couple of problems trying to run the OMAP-L138 in stand-alone. I used to have it working when I just had a 6748 chip but now the ARM will hold the DSP in reset and it doesn't seem to work any longer. I have gone through the sites I have pasted below but none seem to illuminate to me how to load a stand-alone build for just the DSP using Spi. My first problem is that I can't seem to find the u-boot.bin file that is supposed to be in a PSP folder. I've downloaded most of what is on the OMAP Product download page but still don't seem to have that file. Do you know where I could find that?
Also, is there an example somewhere that shows how to load a DSP build or both a DSP and ARM build for stand-alone use (via AISGen)?
Here are the sites I have tried to work with so far:
>http://processors.wiki.ti.com/index.php/Restoring/Flashing_OMAP-L137_Bootloaders
->http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/29355/102075.aspx#102075
->http://processors.wiki.ti.com/index.php/GSG:_OMAP-L138_DVEVM_Additional_Procedures
->Did a cursory E2E search.