Part Number: DRA726
Tool/software: Linux
I need to connect an iPhone to our display thru wifi. No ethernet and no internet access, just connection between the device and the iPhone.
hostap perhaps, if so do you have some good documentation on the one that comes with the automotive yocto?
I need that for a demonstration to some customers, there will be no internet connection and no router available.
I got the device from odroid working as a client with the driver from Rashpberry Pi 4.4 kernel. The one with the TI SDK was not functional.
https://odroidinc.com/products/wifi-module-3
root@actia-global-display:~# lsusb
Bus 004 Device 001: ID 1d6b:0003 Linux Foundation
Bus 003 Device 001: ID 1d6b:0002 Linux Foundation
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation
Bus 001 Device 002: ID 0bda:8176 Realtek Semiconductor Corp. RTL8188CUS 802.11n WLAN Adapter
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation
Michel Catudal
ACTIA Corp