Part Number: AM5728
Tool/software: Linux
Hello again, I've been working on a device tree edit for our custom board, to add some buttons. I have two questions:
1. Since these buttons are going to be used in-application to send messages over ethernet (press button A to send message 1 and button B to send message 2, etc) would the gpio-keys driver be the proper driver? Do the Linux Code values for each pin have to correspond to a value that is available on a keyboard, or are there custom options?
2. If I were to use the gpio-keys or even the sysfs driver, would I be able to see the GPIO change in the u-boot command line interface using gpio status?
Any help would be greatly appreciated :)