Other Parts Discussed in Thread: TVP5158, TVP7002, , DM388
Hi i'm trying to create a video path from HDVPSS capture.
Help request for necessary steps, code or any available documents to configure HDVPSS to capture.
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi i'm trying to create a video path from HDVPSS capture.
Help request for necessary steps, code or any available documents to configure HDVPSS to capture.
Thank you
Hi Anuj, Thank you for the reply.
My source video module consist a customized OMAP -3530 LCD Interface. This is connected to a display using 40 pin flex cable.
The input to the display is 16-bit 422 YCbCr. Y[7:0] available in 8 pins and CbCr[7:0] in other 8 pins. Here I'm removing the display
and the cable interface is latched to the customized carrier card, having TMDSCSK388. It is same like the camera connected with DM388_CSK.
The hardware connections are made such that the input video to the carrier card will reach VIN[0]A port of DM388.
Now the video is connected to VIN port A only,
I have not made any changes in the software IPNC_RDK 3.9.0, It is same as it is for the DM388_CSK application
Thank you.
Hello,
Please find the TVP7002 DS here. TVP7002 is an external IC that can be optionally mounted on your custom carrier board if required.
Thanks
Thank you, Anuj.
I have one doubt, In DM388_CSK (TMDSCSK388 + TMDSCSKCC), the camera is interfaced with the carrier card.
I see the camera inputs directly given to the parallel CAM inputs, so in this case do we not need any video decoders?
As I'm not able to find any decoders in TMDSCSKCC (carrier card).
How is this working?
thank you,
Regards
Hi Nithin,
Can you please share your schematics of your carrier card on my email-id anuj.gupta@pathpartnertech.com.
We will look into to suggest you in a better way.
Hello Nithin,
Hope you have already checked HDVPSS interface details. Please find the link FYR www.ti.com/.../spruhi7a.pdf.
DM38X supports 2 types of Video processing engines namely ISS and HDVPSS. Usually Camera sensors are interfaced to ISS and not to HDVPSS. Please refer HDVPSS data sheet for more details on available interfaces.
Thanks