This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA756: PDK 1.0.5 Potential I2C Driver Issue: I2C transfer always results in I2C_STS_SUCCESS

Part Number: DRA756

There is a potential issue with PDK v.1.0.5.  The IPU I2C driver is always returning I2C_STS_SUCCESS, even if the transfer is not properly ack'd by the slave.  I briefly looked at the release notes for newer Proc-SDK's (with PDK v1.0.6 and v1.0.7) and did not see anything in the fixed issues section.  This can be replicated by just attempting a transfer with the wrong slave address.

Thanks,
Eric