This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: AM335x SDK-06.00 GPMC Prefetch NAND EDMA

Part Number: PROCESSOR-SDK-AM335X

Tool/software: Linux

Hello there,

I have modified some codes to support NAND EDMA,

But something is missed i guess.

Here is the differences:

diff --git a/arch/arm/mach-omap2/board-am335xevm.c b/arch/arm/mach-omap2/board-am335xevm.c
index 9d8a071..fa6be50 100644
--- a/arch/arm/mach-omap2/board-am335xevm.c
+++ b/arch/arm/mach-omap2/board-am335xevm.c
@@ -1325,6 +1325,7 @@ static void evm_nand_init(int evm_id, int profile)
         &am335x_nand_timings);
     if (!pdata)
         return;
+    pdata->xfer_type = NAND_OMAP_PREFETCH_DMA;
     pdata->ecc_opt =OMAP_ECC_BCH8_CODE_HW;
     pdata->elm_used = true;
     gpmc_device[0].pdata = pdata;
diff --git a/drivers/mtd/nand/omap2.c b/drivers/mtd/nand/omap2.c
index deb1c1a..2e33788 100644
--- a/drivers/mtd/nand/omap2.c
+++ b/drivers/mtd/nand/omap2.c
@@ -26,6 +26,9 @@
 #include <plat/nand.h>
 #include <plat/elm.h>
 
+/* some edma specific hacks which might change */
+#include <mach/edma.h>
+
 #define    DRIVER_NAME    "omap2-nand"
 #define    OMAP_NAND_TIMEOUT_MS    5000
 
@@ -366,12 +369,6 @@ static inline int omap_nand_dma_transfer(struct mtd_info *mtd, void *addr,
     int ret;
     unsigned long tim, limit;
 
-    /* The fifo depth is 64 bytes max.
-     * But configure the FIFO-threahold to 32 to get a sync at each frame
-     * and frame length is 32 bytes.
-     */
-    int buf_len = len >> 6;
-
     if (addr >= high_memory) {
         struct page *p1;
 
@@ -392,28 +389,36 @@ static inline int omap_nand_dma_transfer(struct mtd_info *mtd, void *addr,
     }
 
     if (is_write) {
-        omap_set_dma_dest_params(info->dma_ch, 0, OMAP_DMA_AMODE_CONSTANT,
+        omap_set_dma_dest_params(info->dma_ch, 0, OMAP_DMA_AMODE_POST_INC,
                         info->phys_base, 0, 0);
         omap_set_dma_src_params(info->dma_ch, 0, OMAP_DMA_AMODE_POST_INC,
-                            dma_addr, 0, 0);
+                            dma_addr, 4, len);
         omap_set_dma_transfer_params(info->dma_ch, OMAP_DMA_DATA_TYPE_S32,
-                    0x10, buf_len, OMAP_DMA_SYNC_FRAME,
+                    len/4, 1, OMAP_DMA_SYNC_FRAME,
                     OMAP24XX_DMA_GPMC, OMAP_DMA_DST_SYNC);
     } else {
-        omap_set_dma_src_params(info->dma_ch, 0, OMAP_DMA_AMODE_CONSTANT,
+        omap_set_dma_src_params(info->dma_ch, 0, OMAP_DMA_AMODE_POST_INC,
                         info->phys_base, 0, 0);
         omap_set_dma_dest_params(info->dma_ch, 0, OMAP_DMA_AMODE_POST_INC,
-                            dma_addr, 0, 0);
+                            dma_addr, 4, len);
         omap_set_dma_transfer_params(info->dma_ch, OMAP_DMA_DATA_TYPE_S32,
-                    0x10, buf_len, OMAP_DMA_SYNC_FRAME,
+                    len/4, 1, OMAP_DMA_SYNC_FRAME,
                     OMAP24XX_DMA_GPMC, OMAP_DMA_SRC_SYNC);
     }
+#if 0
     /*  configure and start prefetch transfer */
     ret = gpmc_prefetch_enable(info->gpmc_cs,
             PREFETCH_FIFOTHRESHOLD_MAX, 0x1, len, is_write);
     if (ret)
         /* PFPW engine is busy, use cpu copy method */
         goto out_copy;
+#endif
+
+    /* enable interrupts */
+    struct edmacc_param p_ram;
+    edma_read_slot(info->dma_ch, &p_ram);
+    p_ram.opt |= TCINTEN | EDMA_TCC(EDMA_CHAN_SLOT(info->dma_ch));
+    edma_write_slot(info->dma_ch, &p_ram);
 
     init_completion(&info->comp);

So I'm not using GPMC Prefetch, Why can't?

Please HELP me  ; )

  • If I enable GPMC Prefetch, Kernel won't start up, what's the point here?

    [    0.899505] omap-gpmc omap-gpmc: GPMC revision 6.0

    [    0.904510] Registering NAND on CS0

    [    0.909210] _regulator_get: l3_main.0 supply vdd_core not found, using dummy regulator

    [    0.917541] am335x_opp_update: physical regulator not present for core(-22)

    [    0.925018] registered am33xx_sr device

    [    0.930389] mtdoops: mtd device (mtddev=name/number) must be supplied

    [    0.937530] omap2-nand driver initializing

    [    0.941925] omap_set_dma_dest_burst_mode: un-supported SDMA wrapper

    [    0.948455] omap_set_dma_src_burst_mode: un-supported SDMA wrapper

    [    0.955169] NAND device: Manufacturer ID: 0xc2, Chip ID: 0xf1 (Macronix NAND 128MiB 3,3V 8-bit)

    [    0.964385] Creating 1 MTD partitions on "omap2-nand.0":

    [    0.969940] 0x000000000000-0x000008000000 : "File System"

    [    1.026977] OneNAND driver initializing

    [    1.031463] UBI: attaching mtd0 to ubi0

    [    1.035491] UBI: physical eraseblock size:   131072 bytes (128 KiB)

    [    1.041992] UBI: logical eraseblock size:    126976 bytes

    [    1.047637] UBI: smallest flash I/O unit:    2048

    [    1.052520] UBI: VID header offset:          2048 (aligned 2048)

    [    1.058746] UBI: data offset:                4096

    <Here is the END of this, Nothing else>

    And I know is stops at here:

    while (gpmc_read_status(GPMC_PREFETCH_COUNT) && (tim++ < limit))

           cpu_relax();

    It seems that EDMA read data itself, could not using GPMC Prefetch?

  • Hi,

    I see you use board file, so you are using an old kernel (v3.2), right?

    Can you upgrade to latest TISDK, as this is no longer maintained?

    Best Regards,
    Yordan
  • Thanks for your reply.

    Yes, I'm using the old kernel as you say.

    But there is a lot of things to do if  I upgrade to latest TiSDK.

    Now I just want to understand this point, do you have any experience of GPMC Prefetch NAND with EDMA?

    Thank you :)