My customer is finishing up their design with the DM6441 and they are having problems identifying 1.8V NAND Flash that will support this device. They are acessing the NAND via the EMIF I/F and would like as high density as possible, if 2GB is available, they would use it. However, it appears that all or most NAND is now 3.3V and they do not want to add level transition if they dont have to. Please provide 1.8V NAND receommendations for use with the DM6441.