Tool/software: Linux
Hi there, I have followed the steps to partition the SD card and to load the pre-build image to boot Linux on OMAPl138 LCDK.
(followed setps from : )
Following is the error I get while booting :
U-Boot SPL 2017.01-g9fd60700db (Jun 28 2017 - 18:22:04)
Trying to boot from NAND
U-Boot 2017.01-g9fd60700db (Jun 28 2017 - 18:22:04 -0400)
I2C: ready
DRAM: 128 MiB
WARNING: Caches not enabled
NAND: 512 MiB
MMC: davinci: 0
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
Invalid MAC address read.
Net: DaVinci-EMAC
Warning: DaVinci-EMAC (eth0) using random MAC address - 4a:c3:25:2e:6b:57
Hit any key to stop autoboot: 0
Card did not respond to voltage select!
Card did not respond to voltage select!
Card did not respond to voltage select!
Card did not respond to voltage select!