Part Number: AM3352
Tool/software: Linux
Whats the RAM + Flash footprint of the Linux kernel provided in the TI SDK?
BR
Anders Lange
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM3352
Tool/software: Linux
Whats the RAM + Flash footprint of the Linux kernel provided in the TI SDK?
BR
Anders Lange
Make an SD Card and boot a board. Then to see how much flash is used
df -h
To see how much RAM is used
top
Steve K.
Hi Steve.
Thanks for your feedback.
Could you please come up with an estimate.
I do not have the boards to do this...
BR
Anders
Both RAM and flash size depend on what you want to do. The prebuilt tisdk root file system takes up about 1.2GB. There is a much smaller file system that take up less than that. With applications running, the memory used is about 180MB.
Steve K.