This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6657: Power-on sequence leakage on C6657

Part Number: TMS320C6657

Hi all,

I had a custom board using C6657.

We found 650mV leakage from +V1.0_S0_DSP (CVDD1) to +V1.5_S0_DDR3 (DVDD15) supplies during power-up sequencing. Then also make sure a maximum of 100ms between one power rail being valid, and the next power rail in the sequence starting to ramp. Does this negatively impact device operation or reliability?

Thanks in advance.

B.R.

OC