Hi
I'm used to the C55x JTAG interface where you can boot the DSP, then attach your JTAG emulator and connect without having to set the BOOTM pins to emulator boot. This was really helpful since I could load symbols later and set breakpoints.
On the DM648, the CCS can't connect to the EVM without the BOOTM bits set to emulator. Is this a feature of the EVM or is this just how Davinci's work?
Is there a way to connect the JTAG and load symbols after its booted from FLASH (for example).
Thanks