Part Number: TDA2EVM5777
Tool/software: Linux
TDA2EVM5777
software: PROCESSOR_SDK_VISION_03_00_00_00_setuplinux.bin
host hardware: Linux Ubuntu 14.04 64 bit (Ubuntu on a virtual machine)
target hardware: VAYU ES2.0 GP EVM VISION - EVM5777G-03-40-00 703760-1031 REV C
refer VisionSDK_Linux_UserGuide.pdf -> 3.1 Build Linux Vision SDK for Video Capture and Display use-cases -> 4 Run -> SD boot.
and MAKECONFIG=tda2xx_evm_linux_all.
SD card: micro sd 4GB
There are many questions about SD card boot. I need help.
Thank you very much.
U-Boot SPL 2016.05-00002-g1439a4f (Sep 14 2017 - 20:44:19)
DRA752-GP ES2.0
i2c_write: error waiting for addr ACK (status=0x116)
tps65903x: could not set LDO1 voltage.
MMC Device 1 not found
*** Warning - No MMC card found, using default environment
Trying to boot from MMC1
MMC Device 1 not found
*** Warning - No MMC card found, using default environment
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05-00002-g1439a4f (Sep 14 2017 - 20:44:19 -0700)
CPU : DRA752-GP ES2.0
Model: TI DRA742
Board: DRA74x EVM REV H.0
DRAM: 4 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
** First descriptor is NOT a primary desc on 1:1 **
*** Warning - bad CRC, using default environment
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
ERROR: cannot find partition: 'userdata'
at arch/arm/cpu/armv7/omap-common/utils.c:195/mmc_get_part_size()
Warning: fastboot.userdata_size: unable to calc
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net:
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot: 0
i2c_write: error waiting for data ACK (status=0x116)
tps65903x: could not set LDO1 voltage.
switch to partitions #0, OK
mmc0 is current device
i2c_write: error waiting for data ACK (status=0x116)
tps65903x: could not set LDO1 voltage.
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
165 bytes read in 2 ms (80.1 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
i2c_write: error waiting for data ACK (status=0x116)
tps65903x: could not set LDO1 voltage.
switch to partitions #0, OK
mmc0 is current device
i2c_write: error waiting for data ACK (status=0x116)
tps65903x: could not set LDO1 voltage.
SD/MMC found on device 0
3634000 bytes read in 179 ms (19.4 MiB/s)
109715 bytes read in 11 ms (9.5 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x377350 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe2000, end 8ffffc92 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.45-00014-gc08192c-dirty (strong@ubuntu) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #3 SMP PREEMPT Thu Sep 14 20:45:43 PDT 2017
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI DRA742
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000040300000, size 3 MiB
[ 0.000000] Reserved memory: initialized node cmem@40300000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 80 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009e000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a1000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a3000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 64 MiB
[ 0.000000] Reserved memory: initialized node cmem@A9000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0x00000000be400000
[ 0.000000] Forcing write-allocate cache policy for SMP
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] OMAP4: Map 0x00000000bfd00000 to fe600000 for dram barrier
[ 0.000000] DRA752 ES2.0
[ 0.000000] PERCPU: Embedded 11 pages/cpu @ef627000 s14848 r8192 d22016 u45056
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 243264
[ 0.000000] Kernel command line: console=ttyO0,115200n8 vram=16M root=PARTUUID=ea94acf4-02 rw rootwait ip=none mem=1024M
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 328752K/979968K available (6627K kernel code, 371K rwdata, 2492K rodata, 332K init, 290K bss, 446416K reserved, 204800K cma-reserved, 234496K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08f0044 (9121 kB)
[ 0.000000] .init : 0xc08f1000 - 0xc0944000 ( 332 kB)
[ 0.000000] .data : 0xc0944000 - 0xc09a0fd0 ( 372 kB)
[ 0.000000] .bss : 0xc09a2000 - 0xc09ea880 ( 291 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000004] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000015] Switching to timer-based delay loop, resolution 162ns
[ 0.000332] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000340] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000812] Console: colour dummy device 80x30
[ 0.000828] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000834] This ensures that you still see kernel messages. Please
[ 0.000839] update your kernel commandline.
[ 0.000851] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000864] pid_max: default: 32768 minimum: 301
[ 0.000955] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000966] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001499] Initializing cgroup subsys io
[ 0.001516] Initializing cgroup subsys memory
[ 0.001539] Initializing cgroup subsys devices
[ 0.001552] Initializing cgroup subsys freezer
[ 0.001564] Initializing cgroup subsys perf_event
[ 0.001576] Initializing cgroup subsys pids
[ 0.001602] CPU: Testing write buffer coherency: ok
[ 0.001804] /cpus/cpu@0 missing clock-frequency property
[ 0.001820] /cpus/cpu@1 missing clock-frequency property
[ 0.001830] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.001869] Setting up static identity map for 0x80008380 - 0x800083e0
[ 0.080164] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.080225] Brought up 2 CPUs
[ 0.080238] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[ 0.080245] CPU: All CPU(s) started in HYP mode.
[ 0.080250] CPU: Virtualization extensions available.
[ 0.080619] devtmpfs: initialized
[ 0.109881] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.110869] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.206314] omap_hwmod: vpe: no dt node
[ 0.206322] ------------[ cut here ]------------
[ 0.206336] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2523 _init.constprop.23+0x200/0x428()
[ 0.206343] omap_hwmod: vpe: doesn't have mpu register target base
[ 0.206349] Modules linked in:
[ 0.206362] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.4.45-00014-gc08192c-dirty #3
[ 0.206370] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 0.206376] Backtrace:
[ 0.206397] [<c00131b8>] (dump_backtrace) from [<c00133b4>] (show_stack+0x18/0x1c)
[ 0.206405] r7:c08fe01c r6:60000013 r5:00000000 r4:c0970e0c
[ 0.206433] [<c001339c>] (show_stack) from [<c02b4e0c>] (dump_stack+0x8c/0xa0)
[ 0.206445] [<c02b4d80>] (dump_stack) from [<c0034f6c>] (warn_slowpath_common+0x88/0xb8)
[ 0.206451] r7:c08fe01c r6:000009db r5:00000009 r4:ef073e58
[ 0.206474] [<c0034ee4>] (warn_slowpath_common) from [<c0034fd4>] (warn_slowpath_fmt+0x38/0x40)
[ 0.206481] r8:000000ab r7:ef1e86c0 r6:00000000 r5:00000000 r4:c08257b0
[ 0.206506] [<c0034fa0>] (warn_slowpath_fmt) from [<c08fe01c>] (_init.constprop.23+0x200/0x428)
[ 0.206512] r3:c0827a90 r2:c08257b0
[ 0.206523] r4:c0954e98
[ 0.206536] [<c08fde1c>] (_init.constprop.23) from [<c08fe374>] (__omap_hwmod_setup_all+0x48/0x98)
[ 0.206542] r10:00000000 r9:c08f1600 r8:000000ab r7:ef1e86c0 r6:c09496b0 r5:c094bb38
[ 0.206565] r4:c0954e98
[ 0.206577] [<c08fe32c>] (__omap_hwmod_setup_all) from [<c000982c>] (do_one_initcall+0x98/0x1e4)
[ 0.206583] r5:c08fe32c r4:c09496b0
[ 0.206599] [<c0009794>] (do_one_initcall) from [<c08f1f68>] (kernel_init_freeable+0x1d4/0x268)
[ 0.206605] r10:00000002 r9:c08f1600 r8:000000ab r7:c0931820 r6:c093eff4 r5:c09a2000
[ 0.206626] r4:c09a2000
[ 0.206641] [<c08f1d94>] (kernel_init_freeable) from [<c0679ce4>] (kernel_init+0x18/0xf4)
[ 0.206647] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0679ccc
[ 0.206667] r4:c09a2000
[ 0.206681] [<c0679ccc>] (kernel_init) from [<c000fb88>] (ret_from_fork+0x14/0x2c)
[ 0.206687] r5:c0679ccc r4:00000000
[ 0.206710] ---[ end trace eac6d294df07c36b ]---
[ 0.208807] omap_hwmod: wd_timer2: no dt node
[ 0.208814] ------------[ cut here ]------------
[ 0.208825] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2523 _init.constprop.23+0x200/0x428()
[ 0.208832] omap_hwmod: wd_timer2: doesn't have mpu register target base
[ 0.208837] Modules linked in:
[ 0.208848] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 4.4.45-00014-gc08192c-dirty #3
[ 0.208855] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 0.208859] Backtrace:
[ 0.208876] [<c00131b8>] (dump_backtrace) from [<c00133b4>] (show_stack+0x18/0x1c)
[ 0.208882] r7:c08fe01c r6:60000013 r5:00000000 r4:c0970e0c
[ 0.208906] [<c001339c>] (show_stack) from [<c02b4e0c>] (dump_stack+0x8c/0xa0)
[ 0.208917] [<c02b4d80>] (dump_stack) from [<c0034f6c>] (warn_slowpath_common+0x88/0xb8)
[ 0.208923] r7:c08fe01c r6:000009db r5:00000009 r4:ef073e58
[ 0.208944] [<c0034ee4>] (warn_slowpath_common) from [<c0034fd4>] (warn_slowpath_fmt+0x38/0x40)
[ 0.208950] r8:000000ab r7:ef1e86c0 r6:00000000 r5:00000000 r4:c08257b0
[ 0.208974] [<c0034fa0>] (warn_slowpath_fmt) from [<c08fe01c>] (_init.constprop.23+0x200/0x428)
[ 0.208980] r3:c0824ad0 r2:c08257b0
[ 0.208991] r4:c0950018
[ 0.209003] [<c08fde1c>] (_init.constprop.23) from [<c08fe374>] (__omap_hwmod_setup_all+0x48/0x98)
[ 0.209009] r10:00000000 r9:c08f1600 r8:000000ab r7:ef1e86c0 r6:c09496b0 r5:c094bb38
[ 0.209030] r4:c0950018
[ 0.209042] [<c08fe32c>] (__omap_hwmod_setup_all) from [<c000982c>] (do_one_initcall+0x98/0x1e4)
[ 0.209048] r5:c08fe32c r4:c09496b0
[ 0.209063] [<c0009794>] (do_one_initcall) from [<c08f1f68>] (kernel_init_freeable+0x1d4/0x268)
[ 0.209069] r10:00000002 r9:c08f1600 r8:000000ab r7:c0931820 r6:c093eff4 r5:c09a2000
[ 0.209090] r4:c09a2000
[ 0.209103] [<c08f1d94>] (kernel_init_freeable) from [<c0679ce4>] (kernel_init+0x18/0xf4)
[ 0.209109] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0679ccc
[ 0.209129] r4:c09a2000
[ 0.209142] [<c0679ccc>] (kernel_init) from [<c000fb88>] (ret_from_fork+0x14/0x2c)
[ 0.209148] r5:c0679ccc r4:00000000
[ 0.209159] ---[ end trace eac6d294df07c36c ]---
[ 0.320157] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.324347] pinctrl core: initialized pinctrl subsystem
[ 0.325203] NET: Registered protocol family 16
[ 0.326137] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.350229] cpuidle: using governor ladder
[ 0.380260] cpuidle: using governor menu
[ 0.388825] OMAP GPIO hardware version 0.1
[ 0.395331] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[ 0.412176] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 0.412189] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 0.421876] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.421886] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.422352] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.422361] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.422939] OMAP DMA hardware revision 0.0
[ 0.461452] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.462624] edma 43300000.edma: memcpy is disabled
[ 0.467263] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.471565] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.471752] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.471918] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.472083] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.472364] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 0.472567] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 0.475769] palmas 0-0058: IRQ missing: skipping irq request
[ 0.490930] palmas: probe of 0-0058 failed with error -121
[ 0.491573] pcf857x 0-0020: probed
[ 0.492144] pcf857x 0-0021: probed
[ 0.492294] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.510812] pcf857x 1-0026: probed
[ 0.511336] mcp230xx: probe of 1-0027 failed with error -121
[ 0.511559] mcp230xx: probe of 1-0021 failed with error -121
[ 0.511785] mcp230xx: probe of 1-0025 failed with error -121
[ 0.512498] omap_i2c 48072000.i2c: bus 1 rev0.12 at 400 kHz
[ 0.512881] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.513079] media: Linux media interface: v0.10
[ 0.513128] Linux video capture interface: v2.00
[ 0.513165] pps_core: LinuxPPS API ver. 1 registered
[ 0.513172] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.513194] PTP clock support registered
[ 0.513239] EDAC MC: Ver: 3.0.0
[ 0.513980] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.514270] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.514619] Advanced Linux Sound Architecture Driver Initialized.
[ 0.515470] clocksource: Switched to clocksource arch_sys_counter
[ 0.526109] NET: Registered protocol family 2
[ 0.526605] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.526667] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.526792] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.526838] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.526869] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.527075] NET: Registered protocol family 1
[ 0.527316] RPC: Registered named UNIX socket transport module.
[ 0.527325] RPC: Registered udp transport module.
[ 0.527332] RPC: Registered tcp transport module.
[ 0.527339] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.528335] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.530742] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.538345] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.539002] NFS: Registering the id_resolver key type
[ 0.539029] Key type id_resolver registered
[ 0.539037] Key type id_legacy registered
[ 0.539105] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.541083] bounce: pool size: 64 pages
[ 0.541241] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.541258] io scheduler noop registered
[ 0.541273] io scheduler deadline registered
[ 0.541307] io scheduler cfq registered (default)
[ 0.545837] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[ 0.548963] PCI host bridge /ocp/axi@0/pcie_rc@51000000 ranges:
[ 0.548976] No bus range found for /ocp/axi@0/pcie_rc@51000000, using [bus 00-ff]
[ 0.549009] IO 0x20003000..0x20012fff -> 0x00000000
[ 0.549030] MEM 0x20013000..0x2fffffff -> 0x20013000
[ 0.578876] dra7-pcie 51000000.pcie_rc: link is not up
[ 0.579046] dra7-pcie 51000000.pcie_rc: PCI host bridge to bus 0000:00
[ 0.579059] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.579071] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 0.579081] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 0.579484] PCI: bus0: Fast back to back transfers disabled
[ 0.579606] PCI: bus1: Fast back to back transfers enabled
[ 0.579690] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 0.579706] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 0.579719] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.579949] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 0.603390] fpd3_serdes: probe of 7-002c failed with error -5
[ 0.603550] fpd3_serdes 1-001b: Serializer fpd3_24b_ser ready
[ 0.605491] fpd3_serdes 7-002c: Deserializer fpd3_24b_des ready
[ 0.665147] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.668565] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 301, base_baud = 3000000) is a 8250
[ 2.111958] console [ttyS0] enabled
[ 2.116378] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 302, base_baud = 3000000) is a 8250
[ 2.126086] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 303, base_baud = 3000000) is a 8250
[ 2.136131] [drm] Initialized drm 1.1.0 20060810
[ 2.142301] omapdss_dss 58000000.dss: master bind failed: -517
[ 2.149429] connector-hdmi connector@1: failed to find video source
[ 2.171999] loop: module loaded
[ 2.175656] vmemexp device MAJOR num = 246
[ 2.179784] vmemexp class registered
[ 2.183500] /dev/vmemexp device registered
[ 2.187634] ioctl DBUFIOC_EXPORT_VIRTMEM = -1072899120
[ 2.193318] nand: No NAND device found
[ 2.197107] omap2-nand 8000000.nand: scan failed, may be bus-width mismatch
[ 2.206961] m25p80 spi32766.0: s25fl256s1 (32768 Kbytes)
[ 2.212357] 7 ofpart partitions found on MTD device spi32766.0
[ 2.218238] Creating 7 MTD partitions on "spi32766.0":
[ 2.223402] 0x000000000000-0x000000040000 : "QSPI.SPL"
[ 2.229515] 0x000000040000-0x000000140000 : "QSPI.u-boot"
[ 2.235861] 0x000000140000-0x0000001c0000 : "QSPI.u-boot-spl-os"
[ 2.242754] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
[ 2.249429] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
[ 2.256816] 0x0000001e0000-0x0000009e0000 : "QSPI.kernel"
[ 2.263129] 0x0000009e0000-0x000002000000 : "QSPI.file-system"
[ 2.270963] libphy: Fixed MDIO Bus: probed
[ 2.325504] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 2.331629] davinci_mdio 48485000.mdio: detected phy mask fffffff3
[ 2.341822] libphy: 48485000.mdio: probed
[ 2.345894] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver unknown
[ 2.353936] davinci_mdio 48485000.mdio: phy[3]: device 48485000.mdio:03, driver unknown
[ 2.362659] cpsw 48484000.ethernet: Detected MACID = fc:0f:4b:c2:c7:d8
[ 2.369357] cpsw 48484000.ethernet: cpts: overflow check period 800
[ 2.376354] cpsw 48484000.ethernet: cpsw: Detected MACID = fc:0f:4b:c2:c7:d9
[ 2.384930] mousedev: PS/2 mouse device common for all mice
[ 2.391316] i2c /dev entries driver
[ 2.395812] ov1063x 1-0037: Failed writing register 0x0103!
[ 2.401421] ov1063x: probe of 1-0037 failed with error -121
[ 2.407398] ov1063x 1-0030: Failed writing register 0x0103!
[ 2.413006] ov1063x: probe of 1-0030 failed with error -121
[ 2.423632] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 2.456099] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 2.462485] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 2.914692] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.924795] tlv320aic3x-codec 0-0019: Failed to get supply 'IOVDD': -517
[ 2.931575] tlv320aic3x-codec 0-0019: Failed to request supplies: -517
[ 2.939698] davinci-mcasp 4847c000.mcasp: invalid tdm slots: 0
[ 2.947152] NET: Registered protocol family 10
[ 2.952464] sit: IPv6 over IPv4 tunneling driver
[ 2.957697] NET: Registered protocol family 17
[ 2.962379] Key type dns_resolver registered
[ 2.966842] omap_voltage_late_init: Voltage driver support not added
[ 2.973729] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.979957] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.986210] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ 2.992807] Power Management for TI OMAP4+ devices.
[ 2.997988] Registering SWP/SWPB emulation handler
[ 3.005515] dmm 4e000000.dmm: initialized all PAT entries
[ 3.013654] omapdss_dss 58000000.dss: master bind failed: -517
[ 3.019866] connector-hdmi connector@1: failed to find video source
[ 3.026843] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 3.066329] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 3.072715] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 3.105871] tlv320aic3x-codec 0-0019: Failed to get supply 'IOVDD': -517
[ 3.112603] tlv320aic3x-codec 0-0019: Failed to request supplies: -517
[ 3.119860] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 3.126094] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 3.132330] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ 3.139940] input: gpio_keys as /devices/platform/gpio_keys/input/input0
[ 3.146915] hctosys: unable to open rtc device (rtc0)
[ 3.157456] omapdss_dss 58000000.dss: master bind failed: -517
[ 3.163681] connector-hdmi connector@1: failed to find video source
[ 3.166170] evm_3v3_sw: disabling
[ 3.166176] aic_dvdd: disabling
[ 3.166180] vmmcwl_fixed: disabling
[ 3.166190] pbias_mmc_omap5: disabling
[ 3.166203] evm_3v3_sd: disabling
[ 3.166439] ALSA device list:
[ 3.166442] No soundcards found.
[ 3.194288] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 3.225725] Waiting for root device PARTUUID=ea94acf4-02...
[ 3.226483] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 3.226488] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 3.255922] tlv320aic3x-codec 0-0019: Failed to get supply 'IOVDD': -517
[ 3.262656] tlv320aic3x-codec 0-0019: Failed to request supplies: -517
[ 3.269948] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 3.276197] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 3.282436] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517