Part Number: TMS320C6678
Tool/software: Code Composer Studio
Hi TI engineer
In our application there is two C6678 linked to each other by the SRIO(We call it dsp 0 and dsp 1). The link is 4x and 5.0G Baud/s. The reference clock comes from the same source, it's 156.25MHz. When we run our system, sometimes one dsp will meet an error like this:
1. dsp-0 send data to dsp-1, dsp-1 can't receive it. The data length is 64KB, sent from L2 on dsp-0 to MSMC on dsp-1;
2.When the error occurs, dsp-0 get the completion code(from LSU_STAT_REG) , it's equal to 1.Whick means "Transaction Timeout occurred on Non-posted transaction"
3.When the error occurs, we check the ERR_STAT regs(0x0290b158), in dsp 0 it is "0x00010002", in dsp 1 it is"0x00020002". It should both be "0x00020002" in the right case. So we learn that for dsp0, "Output is in the “output error-stopped” state"
4.When the error occurs, we check the ERR_DET regs(0x0290c008), and SP0_ERR_DET regs(0x0290c040).Like this:
ERR_DET SP0_ERR_DET
dsp 0 and dsp 1(right case): 0x0 0x00000010
dsp 0 and dsp 1(wrong case): 0x01000000 0x00100010
So we learn that during the wrong case, both dsp-0 and dsp-1 met "Received packet-not-accepted Control Symbol" and "Packet Response Time-out".
From above we can conclude that during the wrong case, there is something happen in the srio link, whick makes dsp-0 in the output error-stopped state, and can't get packet response in enough time.But we still don't why it will happen. Do you think it is from hardware design or software design?The code to initialize srio is attached .You can check it.
Thank you very much.Looking forward for you reply.
Regards ,Yuchao.
/*
* DrvSrioInit.c
*
* Created on: 2016-3-17
* Author: wangyuchao
*/
#include "Drv_Common.h"
#include "DrvPsc.h"
#include "DrvSrio.h"
#include "DrvSrioStruct.h"
#include "DrvSerdes.h"
#include "DrvTsc.h"
#include <csl_srioAuxPhyLayer.h>
extern CSL_BootcfgRegs *boot_cfg_regs;
CSL_SrioRegs * gp_srioRegs = (CSL_SrioRegs *)CSL_SRIO_CONFIG_REGS;
SerdesRegs * gp_srioSerdesRegs =
(SerdesRegs*)&((CSL_BootcfgRegs*)CSL_BOOT_CFG_REGS)->SRIO_SERDES_CFGPLL;
/*****************************************************************************
Prototype : KeyStone_SRIO_GlobalEnable
Description : enable globally used blocks including MMR block in SRIO
Input : void
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Zhan
Modification : Created function
*****************************************************************************/
void KeyStone_SRIO_GlobalEnable(void)
{
gp_srioRegs->RIO_GBL_EN = 1;
gp_srioRegs->BLOCK_ENABLE_STATUS[0].RIO_BLK_EN= 1; //MMR_EN
//wait for enable completion
while(0x3 != (gp_srioRegs->RIO_GBL_EN_STAT&0x3));
}
/*****************************************************************************
Prototype : KeyStone_SRIO_enable_blocks
Description : Enable SRIO blocks
Input : SRIO_Block_Enable * blockEn
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Brighton Feng
Modification : Created function
*****************************************************************************/
void KeyStone_SRIO_enable_blocks(
SRIO_Block_Enable * blockEn)
{
gp_srioRegs->BLOCK_ENABLE_STATUS[5].RIO_BLK_EN= blockEn->bBLK5_8_Port_Datapath_EN[0];
gp_srioRegs->BLOCK_ENABLE_STATUS[6].RIO_BLK_EN= blockEn->bBLK5_8_Port_Datapath_EN[1];
gp_srioRegs->BLOCK_ENABLE_STATUS[7].RIO_BLK_EN= blockEn->bBLK5_8_Port_Datapath_EN[2];
gp_srioRegs->BLOCK_ENABLE_STATUS[8].RIO_BLK_EN= blockEn->bBLK5_8_Port_Datapath_EN[3];
gp_srioRegs->BLOCK_ENABLE_STATUS[1].RIO_BLK_EN= blockEn->bBLK1_LSU_EN ;
gp_srioRegs->BLOCK_ENABLE_STATUS[2].RIO_BLK_EN= blockEn->bBLK2_MAU_EN ;
gp_srioRegs->BLOCK_ENABLE_STATUS[3].RIO_BLK_EN= blockEn->bBLK3_TXU_EN ;
gp_srioRegs->BLOCK_ENABLE_STATUS[4].RIO_BLK_EN= blockEn->bBLK4_RXU_EN ;
while(gp_srioRegs->BLOCK_ENABLE_STATUS[5].RIO_BLK_EN_STAT != blockEn->bBLK5_8_Port_Datapath_EN[0]);
while(gp_srioRegs->BLOCK_ENABLE_STATUS[6].RIO_BLK_EN_STAT != blockEn->bBLK5_8_Port_Datapath_EN[1]);
while(gp_srioRegs->BLOCK_ENABLE_STATUS[7].RIO_BLK_EN_STAT != blockEn->bBLK5_8_Port_Datapath_EN[2]);
while(gp_srioRegs->BLOCK_ENABLE_STATUS[8].RIO_BLK_EN_STAT != blockEn->bBLK5_8_Port_Datapath_EN[3]);
while(gp_srioRegs->BLOCK_ENABLE_STATUS[1].RIO_BLK_EN_STAT != blockEn->bBLK1_LSU_EN );
while(gp_srioRegs->BLOCK_ENABLE_STATUS[2].RIO_BLK_EN_STAT != blockEn->bBLK2_MAU_EN );
while(gp_srioRegs->BLOCK_ENABLE_STATUS[3].RIO_BLK_EN_STAT != blockEn->bBLK3_TXU_EN );
while(gp_srioRegs->BLOCK_ENABLE_STATUS[4].RIO_BLK_EN_STAT != blockEn->bBLK4_RXU_EN );
}
void SRIO_HyperLink_Serdes_init(SerdesSetup_4links* serdes_cfg, SerdesRegs* serdesRegs)
{
int i;
float pllMpy, serdesPllClock_GHz=12.5, rateScale;
SerdesLinkRate linkRateScale;
SerdesVcoRange vcoRange;
Uint32 CFGTX;
if(NULL== serdes_cfg)
return;
CSL_BootCfgUnlockKicker();
/*find lowest link speed, the SERDES PLL output should be less or equal to it*/
for(i= 0; i<4; i++)
{
if(serdes_cfg->linkSetup[i])
if(serdesPllClock_GHz >serdes_cfg->linkSetup[i]->linkSpeed_GHz)
serdesPllClock_GHz = serdes_cfg->linkSetup[i]->linkSpeed_GHz;
}
/*Serdes PLL output must be between 1.5625 and 3.125*/
if(serdesPllClock_GHz>6.25)
serdesPllClock_GHz /= 4;
else if(serdesPllClock_GHz>3.125)
serdesPllClock_GHz /= 2;
else if(serdesPllClock_GHz<1.5625)
serdesPllClock_GHz *= 2;
else
;
/*set VCO range according to the PLL output speed*/
if(serdesPllClock_GHz<2.17)
vcoRange= SERDES_PLL_VCO_RANGE_HIGH;
else
vcoRange= SERDES_PLL_VCO_RANGE_LOW;
pllMpy = serdesPllClock_GHz*1000/serdes_cfg->commonSetup.inputRefClock_MHz;
/*PLL multiply factors between 4 and 60*/
pllMpy = (pllMpy<4 || pllMpy>60)?4:pllMpy;
serdesRegs->CFGPLL = (1<<SERDES_PLL_CFG_ENPLL_SHIFT)|
(serdes_cfg->commonSetup.loopBandwidth<<SERDES_PLL_CFG_LOOPBANDWIDTH_SHIFT)|
(vcoRange<<SERDES_PLL_CFG_VRANGE_SHIFT)|
((Uint32)(pllMpy*4)<<SERDES_PLL_CFG_MPY_SHIFT);
for(i=0; i<4; i++)
{
if(serdes_cfg->linkSetup[i])
{
rateScale = 1.0;
rateScale=serdes_cfg->linkSetup[i]->linkSpeed_GHz/serdesPllClock_GHz;
if(rateScale<1)
linkRateScale = SRIO_SERDES_LINK_RATE_div2;
else if(rateScale<2)
linkRateScale = SRIO_SERDES_LINK_RATE_x1;
else if(rateScale<4)
linkRateScale = SRIO_SERDES_LINK_RATE_x2;
else
linkRateScale = SRIO_SERDES_LINK_RATE_x4;
serdesRegs->link[i].CFGRX= (1<<SERDES_RX_CFG_ENRX_SHIFT)|
(2<<SERDES_RX_CFG_BUSWIDTH_SHIFT)| /*Bus width must be 010b (20 bit)*/
(serdes_cfg->linkSetup[i]->testPattern<<SERDES_RX_CFG_TESTPATTERN_SHIFT)|
(serdes_cfg->linkSetup[i]->loopBack<<SERDES_RX_CFG_LOOPBACK_SHIFT)|
(1<<SERDES_RX_CFG_ENOC_SHIFT)| /*Enable offset compensation*/
(serdes_cfg->linkSetup[i]->rxEqualizerConfig<<SERDES_RX_CFG_EQ_SHIFT)|
(serdes_cfg->linkSetup[i]->rxCDR<<SERDES_RX_CFG_CDR_SHIFT)|
(serdes_cfg->linkSetup[i]->rxLos<<SERDES_RX_CFG_LOS_SHIFT)|
(serdes_cfg->linkSetup[i]->rxAlign<<SERDES_RX_CFG_ALIGN_SHIFT)|
(serdes_cfg->linkSetup[i]->rxTermination<<SERDES_RX_CFG_TERM_SHIFT)|
(serdes_cfg->linkSetup[i]->rxInvertPolarity<<SERDES_RX_CFG_INVPAIR_SHIFT)|
(linkRateScale<<SERDES_RX_CFG_RATE_SHIFT);
CFGTX= (1<<SERDES_TX_CFG_ENTX_SHIFT)|
(2<<SERDES_TX_CFG_BUSWIDTH_SHIFT)| /*Bus width must be 010b (20 bit)*/
(serdes_cfg->linkSetup[i]->testPattern<<SERDES_TX_CFG_TESTPATTERN_SHIFT)|
(serdes_cfg->linkSetup[i]->loopBack<<SERDES_TX_CFG_LOOPBACK_SHIFT)|
(1<<SERDES_TX_CFG_FIRUPT_SHIFT)| /*FIRUPT = 1 Transmitter pre and post cursor FIR filter update*/
/*TWPST1: Adjacent Post Cursor Tap Weight.
If trace length is 4��, start with 20 (-10%).
If trace length is between 4�� and 10��, start with 27 (-27.5%).*/
// (18<<SERDES_TX_CFG_TWPST1_SHIFT)|
// (1<<SERDES_TX_CFG_TWPRE_SHIFT)| /*TWPRE: The settings range from 0 to -17.5% in 2.5% steps.*/
(serdes_cfg->linkSetup[i]->txOutputSwing<<SERDES_TX_CFG_SWING_SHIFT)|
(serdes_cfg->linkSetup[i]->txInvertPolarity<<SERDES_TX_CFG_INVPAIR_SHIFT)|
(linkRateScale<<SERDES_TX_CFG_RATE_SHIFT);
if(i==0) //lane 0 is Synchronization
serdesRegs->link[i].CFGTX= CFGTX|
(1<<SERDES_TX_CFG_MYSNC_SHIFT);
else
serdesRegs->link[i].CFGTX= CFGTX|
(0<<SERDES_TX_CFG_MYSNC_SHIFT);
}
}
}
/*****************************************************************************
Prototype : KeyStone_SRIO_set_1x2x4x_Path
Description : configure SRIO 1x 2x or 4x path mode
Input : SRIO_1x2x4x_Path_Control srio_1x2x4x_path_control
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Brighton Feng
Modification : Created function
*****************************************************************************/
void KeyStone_SRIO_set_1x2x4x_Path(
SRIO_1x2x4x_Path_Control srio_1x2x4x_path_control)
{
/*This register is a global register, even though it can be accessed
from any port. So you do not need to program from each port, it is
basically a single register.
The PathID is a RO value, that is driven by the H/W. You cannot modify it*/
gp_srioRegs->RIO_PLM[0].RIO_PLM_SP_PATH_CTL=
(gp_srioRegs->RIO_PLM[0].RIO_PLM_SP_PATH_CTL&(~SRIO_1x2x4x_PATH_CONTROL_MASK))|
srio_1x2x4x_path_control;
}
/*****************************************************************************
Prototype : KeyStone_SRIO_set_device_ID
Description : configure SRIO device ID
Input : SRIO_Device_ID_Routing_Config * device_id_routing_config
Uint32 uiDeviceIdNum
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Brighton Feng
Modification : Created function
*****************************************************************************/
void KeyStone_SRIO_set_device_ID(
SRIO_Device_ID_Routing_Config * device_id_routing_config,
Uint32 uiDeviceIdNum)
{
int i;
/*The TLM_SP(n)_BRR_x_PATTERN_MATCH registers hold the 15 allowable DestIDs,
note that the first register is not used. We use the RIO_BASE_ID register
to hold the first ID */
gp_srioRegs->RIO_BASE_ID= device_id_routing_config[0].idPattern| /*Large ID*/
((device_id_routing_config[0].idPattern&0xFF)<<16); /*small ID*/
/*The host base device ID lock CSR contains the base device ID value for
the processing element in the system that is responsible for initializing
this processing element.*/
gp_srioRegs->RIO_HOST_BASE_ID_LOCK =
device_id_routing_config[0].idPattern;
uiDeviceIdNum= _min2(SRIO_MAX_DEVICEID_NUM, uiDeviceIdNum);
for(i= 1; i<uiDeviceIdNum; i++)
{
/*please note, SRIO block 5~8 must be eanbled for corresponding
RIO_TLM[0:3] taking effect*/
gp_srioRegs->RIO_TLM[i/4].brr[i&3].RIO_TLM_SP_BRR_CTL =
(device_id_routing_config[i].routeMaintenance<<
CSL_SRIO_RIO_TLM_SP_BRR_1_CTL_ROUTE_MR_TO_LLM_SHIFT)|
(0<<CSL_SRIO_RIO_TLM_SP_BRR_1_CTL_PRIVATE_SHIFT)|
(1<<CSL_SRIO_RIO_TLM_SP_BRR_1_CTL_ENABLE_SHIFT);
gp_srioRegs->RIO_TLM[i/4].brr[i&3].RIO_TLM_SP_BRR_PATTERN_MATCH =
(device_id_routing_config[i].idPattern<<
CSL_SRIO_RIO_TLM_SP_BRR_1_PATTERN_MATCH_PATTERN_SHIFT)|
(device_id_routing_config[i].idMatchMask<<
CSL_SRIO_RIO_TLM_SP_BRR_1_PATTERN_MATCH_MATCH_SHIFT);
}
}
/*****************************************************************************
Prototype : KeyStone_SRIO_CSR_CAR_Config
Description : configure SRIO standard Command Status Capability registers
Input : SRIO_Config * srio_cfg
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Brighton Feng
Modification : Created function
*****************************************************************************/
void KeyStone_SRIO_CSR_CAR_Config(SRIO_Config * srio_cfg)
{
int i;
Uint32 uiRegisterValue;
Uint32 uiSpeed_MHz;
gp_srioRegs->RIO_DEV_ID = (0x009D << CSL_SRIO_RIO_DEV_ID_DEV_ID_SHIFT)
|(0x0030 << CSL_SRIO_RIO_DEV_ID_DEV_VEN_ID_SHIFT);
/*The lower 4b should match the 4b from the JTAG Variant field of
the DeviceID register.*/
gp_srioRegs->RIO_DEV_INFO = boot_cfg_regs->DEVICE_ID_REG0>>28;
gp_srioRegs->RIO_PE_FEAT =
(0 << CSL_SRIO_RIO_PE_FEAT_BRDG_SHIFT) /*PE is not a bridge*/
|(0 << CSL_SRIO_RIO_PE_FEAT_MEM_SHIFT) /*PE is not a memory*/
|(1 << CSL_SRIO_RIO_PE_FEAT_PROC_SHIFT) /*PE is a processor*/
|(0 << CSL_SRIO_RIO_PE_FEAT_SW_SHIFT) /*PE is not a switch*/
|(0 << CSL_SRIO_RIO_PE_FEAT_MULT_P_SHIFT) //???
|(0 << CSL_SRIO_RIO_PE_FEAT_FLOW_ARB_SHIFT) //???
|(0 << CSL_SRIO_RIO_PE_FEAT_MC_SHIFT) //???
|(0 << CSL_SRIO_RIO_PE_FEAT_ERTC_SHIFT) //???
|(1 << CSL_SRIO_RIO_PE_FEAT_SRTC_SHIFT) //???
|(1 << CSL_SRIO_RIO_PE_FEAT_FLOW_CTRL_SHIFT)/*PE supports flow control*/
|(1 << 6) //???
|(1 << CSL_SRIO_RIO_PE_FEAT_CRF_SHIFT) /*PE supports CRF Function*/
|(1 << CSL_SRIO_RIO_PE_FEAT_CTLS_SHIFT) /*supports common transport large systems*/
|(1 << CSL_SRIO_RIO_PE_FEAT_EXT_FEA_SHIFT) /*PE has extended features list*/
|(1 << CSL_SRIO_RIO_PE_FEAT_EXT_AS_SHIFT); /*PE supports 34 bit addresses*/
gp_srioRegs->RIO_SW_PORT = (0 << CSL_SRIO_RIO_SW_PORT_PORT_TOTAL_SHIFT) //???
|(4 << CSL_SRIO_RIO_SW_PORT_PORT_NUM_SHIFT); //???
gp_srioRegs->RIO_SRC_OP =
(0 << CSL_SRIO_RIO_SRC_OP_G_READ_SHIFT) //???
|(0 << CSL_SRIO_RIO_SRC_OP_G_IREAD_SHIFT) //???
|(0 << CSL_SRIO_RIO_SRC_OP_G_READ_OWN_SHIFT)//???
|(0 << CSL_SRIO_RIO_SRC_OP_G_DC_INVALIDATE_SHIFT) //???
|(0 << CSL_SRIO_RIO_SRC_OP_G_CASTOUT_SHIFT) //???
|(0 << CSL_SRIO_RIO_SRC_OP_G_DC_FLUSH_SHIFT) //???
|(0 << CSL_SRIO_RIO_SRC_OP_G_IO_READ_SHIFT) //???
|(0 << CSL_SRIO_RIO_SRC_OP_G_IC_INVALIDATE_SHIFT) //???
|(0 << CSL_SRIO_RIO_SRC_OP_G_TLB_INVALIDATE_SHIFT) //???
|(0 << CSL_SRIO_RIO_SRC_OP_G_TLB_SYNC_SHIFT) //???
|(0 << CSL_SRIO_RIO_SRC_OP_G_RIO_RSVD_10_SHIFT) //???
|(0 << CSL_SRIO_RIO_SRC_OP_G_RIO_RSVD_11_SHIFT) //???
|(0 << CSL_SRIO_RIO_SRC_OP_DS_TM_SHIFT) //???
|(1 << CSL_SRIO_RIO_SRC_OP_DS_SHIFT) //???
|(0 << CSL_SRIO_RIO_SRC_OP_IMPLEMENT_DEF_SHIFT) //???
|(1 << CSL_SRIO_RIO_SRC_OP_READ_SHIFT) /*support a read operation*/
|(1 << CSL_SRIO_RIO_SRC_OP_WRITE_SHIFT) /*support a write operation*/
|(1 << CSL_SRIO_RIO_SRC_OP_STRM_WR_SHIFT) /*support a streaming write operation*/
|(1 << CSL_SRIO_RIO_SRC_OP_WR_RES_SHIFT) /*support a write with response operation*/
|(1 << CSL_SRIO_RIO_SRC_OP_D_MSG_SHIFT) /*support a data message operation*/
|(1 << CSL_SRIO_RIO_SRC_OP_DBELL_SHIFT) /*support a doorbell operation*/
|(0 << CSL_SRIO_RIO_SRC_OP_ACSWAP_SHIFT) //???
|(1 << CSL_SRIO_RIO_SRC_OP_ATSWAP_SHIFT) /*support an atomic test-and-swap operation*/
|(1 << CSL_SRIO_RIO_SRC_OP_A_INC_SHIFT) /*support an atomic increment operation*/
|(1 << CSL_SRIO_RIO_SRC_OP_A_DEC_SHIFT) /*support an atomic decrement operation*/
|(1 << CSL_SRIO_RIO_SRC_OP_A_SET_SHIFT) /*support an atomic set operation*/
|(1 << CSL_SRIO_RIO_SRC_OP_A_CLEAR_SHIFT) /*support an atomic clear operation*/
|(0 << CSL_SRIO_RIO_SRC_OP_A_SWAP_SHIFT) //???
|(1 << CSL_SRIO_RIO_SRC_OP_PORT_WR_SHIFT) /*support a port-write generation*/
|(0 << CSL_SRIO_RIO_SRC_OP_IMPLEMENT_DEF2_SHIFT); //??? 0x0004FDF4;
gp_srioRegs->RIO_DEST_OP =
(0 << CSL_SRIO_RIO_DEST_OP_G_READ_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_G_IREAD_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_G_READ_OWN_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_G_DC_INVALIDATE_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_G_CASTOUT_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_G_DC_FLUSH_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_G_IO_READ_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_G_IC_INVALIDATE_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_G_TLB_INVALIDATE_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_G_TLB_SYNC_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_G_RIO_RSVD_10_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_G_RIO_RSVD_11_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_DS_TM_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_DS_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_IMPLEMENT_DEF_SHIFT) //???
|(1 << CSL_SRIO_RIO_DEST_OP_READ_SHIFT) /*support a read operation*/
|(1 << CSL_SRIO_RIO_DEST_OP_WRITE_SHIFT) /*support a write operation*/
|(1 << CSL_SRIO_RIO_DEST_OP_STRM_WR_SHIFT) /*support a streaming write operation*/
|(1 << CSL_SRIO_RIO_DEST_OP_WR_RES_SHIFT) /*support a write with response operation*/
|(1 << CSL_SRIO_RIO_DEST_OP_D_MSG_SHIFT) /*support a data message operation*/
|(1 << CSL_SRIO_RIO_DEST_OP_DBELL_SHIFT) /*support a doorbell operation*/
|(0 << CSL_SRIO_RIO_DEST_OP_ACSWAP_SHIFT) //???
|(0 << CSL_SRIO_RIO_DEST_OP_ATSWAP_SHIFT) /*support an atomic test-and-swap operation*/
|(0 << CSL_SRIO_RIO_DEST_OP_A_INC_SHIFT) /*support an atomic increment operation*/
|(0 << CSL_SRIO_RIO_DEST_OP_A_DEC_SHIFT) /*support an atomic decrement operation*/
|(0 << CSL_SRIO_RIO_DEST_OP_A_SET_SHIFT) /*support an atomic set operation*/
|(0 << CSL_SRIO_RIO_DEST_OP_A_CLEAR_SHIFT) /*support an atomic clear operation*/
|(0 << CSL_SRIO_RIO_DEST_OP_A_SWAP_SHIFT) //???
|(1 << CSL_SRIO_RIO_DEST_OP_PORT_WR_SHIFT) /*support a port-write operation*/
|(0 << CSL_SRIO_RIO_DEST_OP_IMPLEMENT_DEF2_SHIFT); //??? 0x0000FC04;
/*PE supports 34 bit addresses*/
gp_srioRegs->RIO_PE_LL_CTL= (1<<CSL_SRIO_RIO_PE_LL_CTL_EXT_ADDR_CTL_SHIFT);
/*Software defined component tag for the PE.
Useful for devices without device IDs.*/
gp_srioRegs->RIO_COMP_TAG = 0 ; // not touched
/* port general control */
gp_srioRegs->RIO_SP_GEN_CTL = // agent, master, undiscovered
(0 << CSL_SRIO_RIO_SP_GEN_CTL_HOST_SHIFT)
|(1 << CSL_SRIO_RIO_SP_GEN_CTL_MAST_EN_SHIFT)
|(0 << CSL_SRIO_RIO_SP_GEN_CTL_DISC_SHIFT);
/*port control*/
for(i= 0; i< SRIO_MAX_PORT_NUM; i++)
{
if(FALSE==srio_cfg->blockEn.bLogic_Port_EN[i])
continue;
uiRegisterValue=
(0<<CSL_SRIO_RIO_SP_CTL_PORT_DIS_SHIFT )
|(1<<CSL_SRIO_RIO_SP_CTL_OTP_EN_SHIFT )
|(1<<CSL_SRIO_RIO_SP_CTL_INP_EN_SHIFT )
|(0<<CSL_SRIO_RIO_SP_CTL_STOP_FAIL_EN_SHIFT)
|(1<<CSL_SRIO_RIO_SP_CTL_PTYP_SHIFT );
if(NULL!=srio_cfg->flowControlID)
uiRegisterValue|=
(1<<CSL_SRIO_RIO_SP_CTL_FLOW_CTRL_SHIFT )
|(1<<CSL_SRIO_RIO_SP_CTL_FLOW_ARB_SHIFT );
gp_srioRegs->RIO_SP[i].RIO_SP_CTL = uiRegisterValue;
uiSpeed_MHz= (Uint32)(srio_cfg->serdes_cfg->linkSetup[i]->linkSpeed_GHz*1000);
if(1250==uiSpeed_MHz)
gp_srioRegs->RIO_SP[i].RIO_SP_CTL2 =
1<<CSL_SRIO_RIO_SP_CTL2_GB_1P25_EN_SHIFT;
if(2500==uiSpeed_MHz)
gp_srioRegs->RIO_SP[i].RIO_SP_CTL2 =
1<<CSL_SRIO_RIO_SP_CTL2_GB_2P5_EN_SHIFT;
if(3125==uiSpeed_MHz)
gp_srioRegs->RIO_SP[i].RIO_SP_CTL2 =
1<<CSL_SRIO_RIO_SP_CTL2_GB_3P125_EN_SHIFT;
if(5000==uiSpeed_MHz)
gp_srioRegs->RIO_SP[i].RIO_SP_CTL2 =
1<<CSL_SRIO_RIO_SP_CTL2_GB_5P0_EN_SHIFT;
if(6250==uiSpeed_MHz)
gp_srioRegs->RIO_SP[i].RIO_SP_CTL2 =
1<<CSL_SRIO_RIO_SP_CTL2_GB_6P25_EN_SHIFT;
/*disable port write*/
gp_srioRegs->RIO_PLM[i].RIO_PLM_SP_ALL_PW_EN = 0;
}
/*clear port write dest Id, port write not used*/
gp_srioRegs->RIO_PW_TGT_ID= 0;
/*disable port write*/
gp_srioRegs->RIO_EM_DEV_PW_EN = 0;
/* Register Reset Control
Allows the SELF_RST and PWDN_PORT resets to clear sticky register bits
in addition to the normal configuration registers.*/
gp_srioRegs->RIO_REG_RST_CTL =
1 << CSL_SRIO_RIO_REG_RST_CTL_CLEAR_STICKY_SHIFT;
}
/*****************************************************************************
Prototype : KeyStone_SRIO_Error_Capture_Enable
Description : enable error capture for SRIO
Input : SRIO_Block_Enable * blockEn
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Brighton Feng
Modification : Created function
*****************************************************************************/
void KeyStone_SRIO_Error_Capture_Enable(SRIO_Block_Enable * blockEn)
{
Int32 i;
/*Enable specific error reporting, save and lock capture information
in the appropriate Logical/Transport Layer Capture CSRs*/
gp_srioRegs->RIO_ERR_EN=
(1 << CSL_SRIO_RIO_ERR_EN_IO_ERR_RESP_EN_SHIFT) /*"ERROR" response for an direct IO*/
|(1 << CSL_SRIO_RIO_ERR_EN_MSG_ERR_RESP_EN_SHIFT) /*"ERROR" response for an message*/
|(0 << CSL_SRIO_RIO_ERR_EN_GSM_ERR_RESP_EN_SHIFT)
|(1 << CSL_SRIO_RIO_ERR_EN_MSG_FMT_ERR_EN_SHIFT) /*received message with invalid fromat*/
|(1 << CSL_SRIO_RIO_ERR_EN_ILL_TRANS_DECODE_EN_SHIFT) /*Illegal transaction decode*/
|(1 << CSL_SRIO_RIO_ERR_EN_ILL_TRANS_TGT_ERR_EN_SHIFT) /*Illegal transaction target error*/
|(1 << CSL_SRIO_RIO_ERR_EN_MSG_REQ_TIMEOUT_EN_SHIFT) /*Message Request Time-out*/
|(1 << CSL_SRIO_RIO_ERR_EN_PKT_RESP_TIMEOUT_EN_SHIFT) /*Packet Response Time-out*/
|(1 << CSL_SRIO_RIO_ERR_EN_UNSOLICITED_RESP_EN_SHIFT) /*unsolicited/unexpected Response*/
|(1 << CSL_SRIO_RIO_ERR_EN_UNSUPPORTED_TRANS_EN_SHIFT) /*Unsupported Transaction*/
|(1 << CSL_SRIO_RIO_ERR_EN_PDU_LEN_ERR_EN_SHIFT) /*Data streaming PDU length error*/
|(1 << CSL_SRIO_RIO_ERR_EN_SHORT_STREAM_SEG_EN_SHIFT) /*Short data streaming segment*/
|(1 << CSL_SRIO_RIO_ERR_EN_LONG_STREAM_SEG_EN_SHIFT) /*Long data streaming segment*/
|(1 << CSL_SRIO_RIO_ERR_EN_OPEN_STREAM_CONTEXT_EN_SHIFT) /*Open existing data streaming context*/
|(1 << CSL_SRIO_RIO_ERR_EN_MISSING_STREAM_CONTEXT_EN_SHIFT) /*Missing data streaming context*/
|(1 << CSL_SRIO_RIO_ERR_EN_CPPI_SECURITY_VIOLATION_EN_SHIFT)/*RX CPPI Security Violation*/
|(1 << CSL_SRIO_RIO_ERR_EN_RX_DMA_ERR_EN_SHIFT); /*RX I/O DMA Access Error*/
/*Error detect register, write 0 to clear it.*/
gp_srioRegs->RIO_ERR_DET= 0 ;
/*clear error capture registers*/
gp_srioRegs->RIO_H_ADDR_CAPT= 0;
gp_srioRegs->RIO_ADDR_CAPT= 0 ;
gp_srioRegs->RIO_ID_CAPT= 0 ;
gp_srioRegs->RIO_CTRL_CAPT= 0;
//enable physical layer error capture
for(i=0; i< SRIO_MAX_PORT_NUM; i++)
{
if(FALSE == blockEn->bLogic_Port_EN[i])
continue;
/*Enable error rate counting*/
gp_srioRegs->RIO_SP_ERR[i].RIO_SP_RATE_EN=
(1<<CSL_SRIO_RIO_SP_RATE_EN_IMP_SPEC_EN_SHIFT )
|(1<<CSL_SRIO_RIO_SP_RATE_EN_CS_CRC_EN_SHIFT )
|(1<<CSL_SRIO_RIO_SP_RATE_EN_CS_ILL_ID_EN_SHIFT )
|(1<<CSL_SRIO_RIO_SP_RATE_EN_CS_NOT_ACC_EN_SHIFT )
|(1<<CSL_SRIO_RIO_SP_RATE_EN_PKT_ILL_ACKID_EN_SHIFT)
|(1<<CSL_SRIO_RIO_SP_RATE_EN_PKT_CRC_ERR_EN_SHIFT )
|(1<<CSL_SRIO_RIO_SP_RATE_EN_PKT_ILL_SIZE_EN_SHIFT )
|(1<<CSL_SRIO_RIO_SP_RATE_EN_DSCRAM_LOS_EN_SHIFT )
|(1<<CSL_SRIO_RIO_SP_RATE_EN_LR_ACKID_ILL_EN_SHIFT )
|(1<<CSL_SRIO_RIO_SP_RATE_EN_PROT_ERR_EN_SHIFT )
|(1<<CSL_SRIO_RIO_SP_RATE_EN_DELIN_ERR_EN_SHIFT )
|(1<<CSL_SRIO_RIO_SP_RATE_EN_CS_ACK_ILL_EN_SHIFT )
|(1<<CSL_SRIO_RIO_SP_RATE_EN_LINK_TO_EN_SHIFT );
/*the threshold value for reporting an error condition*/
gp_srioRegs->RIO_SP_ERR[i].RIO_SP_ERR_THRESH=
(0xF<<CSL_SRIO_RIO_SP_ERR_THRESH_ERR_RFT_SHIFT)
|(0x4<<CSL_SRIO_RIO_SP_ERR_THRESH_ERR_RDT_SHIFT);
/*Error detect register, write 0 to clear it.*/
gp_srioRegs->RIO_SP_ERR[i].RIO_SP_ERR_DET= 0;
/*clear error capture registers*/
gp_srioRegs->RIO_SP_ERR[i].RIO_SP_ERR_ATTR_CAPT= 0;
gp_srioRegs->RIO_SP_ERR[i].RIO_SP_ERR_CAPT_0= 0;
gp_srioRegs->RIO_SP_ERR[i].RIO_SP_ERR_CAPT_1= 0;
gp_srioRegs->RIO_SP_ERR[i].RIO_SP_ERR_CAPT_2= 0;
gp_srioRegs->RIO_SP_ERR[i].RIO_SP_ERR_CAPT_3= 0;
/*clear error rate counter*/
gp_srioRegs->RIO_SP_ERR[i].RIO_SP_ERR_RATE= 0;
/*read this register to clear the error count in it*/
i = gp_srioRegs->RIO_LANE[i].RIO_LANE_STAT0;
#if 0
gp_srioRegs->RIO_PORT_OPTION[i].SP_CTL_INDEP= gp_srioRegs->PORT_OPTION[i].SP_CTL_INDEP|
(CSL_SRIO_SP_CTL_INDEP_ILL_TRANS_EN_ENABLE<<CSL_SRIO_SP_CTL_INDEP_ILL_TRANS_EN_SHIFT)|
(CSL_SRIO_SP_CTL_INDEP_MAX_RETRY_EN_ENABLE<<CSL_SRIO_SP_CTL_INDEP_MAX_RETRY_EN_SHIFT)|
(255<<CSL_SRIO_SP_CTL_INDEP_MAX_RETRY_THR_SHIFT)|
(CSL_SRIO_SP_CTL_INDEP_IRQ_EN_ENABLE<<CSL_SRIO_SP_CTL_INDEP_IRQ_EN_SHIFT);
#endif
}
}
/*****************************************************************************
Prototype : KeyStone_SRIO_RxMode_Setup
Description : Rx Mode configuration
Input : SRIO_RX_Mode * rxMode
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Brighton Feng
Modification : Created function
*****************************************************************************/
void KeyStone_SRIO_RxMode_Setup(SRIO_RX_Mode * rxMode)
{
int i;
if(rxMode)
{
gp_srioRegs->RIO_PER_SET_CNTL = (gp_srioRegs->RIO_PER_SET_CNTL&
(~CSL_SRIO_RIO_PER_SET_CNTL_LOG_TGT_ID_DIS_MASK))|
(rxMode->accept_data_with_any_ID
<<CSL_SRIO_RIO_PER_SET_CNTL_LOG_TGT_ID_DIS_SHIFT);
/*set RX mode for all ports*/
for(i=0; i<SRIO_MAX_PORT_NUM; i++)
{
gp_srioRegs->RIO_TLM[i].RIO_TLM_SP_CONTROL =
(gp_srioRegs->RIO_TLM[i].RIO_TLM_SP_CONTROL&
(~(CSL_SRIO_RIO_TLM_SP_CONTROL_TGT_ID_DIS_MASK
|CSL_SRIO_RIO_TLM_SP_CONTROL_MTC_TGT_ID_DIS_MASK)))
|(rxMode->port_rx_mode[i].accept_maintenance_with_any_ID
<<CSL_SRIO_RIO_TLM_SP_CONTROL_MTC_TGT_ID_DIS_SHIFT)
|(rxMode->port_rx_mode[i].support_multicast_forwarding
<<CSL_SRIO_RIO_TLM_SP_CONTROL_TGT_ID_DIS_SHIFT);
}
}
}
/*****************************************************************************
Prototype : KeyStone_SRIO_packet_forwarding_Cfg
Description : configure SRIO packet forwarding
Input : SRIO_PktForwarding_Cfg * PktForwardingEntry_cfg
Uint32 pktForwardingEntryNum
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Brighton Feng
Modification : Created function
*****************************************************************************/
void KeyStone_SRIO_packet_forwarding_Cfg(
SRIO_PktForwarding_Cfg * PktForwardingEntry_cfg,
Uint32 pktForwardingEntryNum)
{
int i = 0;
pktForwardingEntryNum= _min2(SRIO_MAX_FORWARDING_ENTRY_NUM,
pktForwardingEntryNum);
for(i=0; i<pktForwardingEntryNum; i++)
{
gp_srioRegs->PF_CNTL[i].RIO_PF_16B_CNTL =
(PktForwardingEntry_cfg[i].forwardingID_up_16
<< CSL_SRIO_RIO_PF_16B_CNTL_DEVID_16B_UP_SHIFT)
|(PktForwardingEntry_cfg[i].forwardingID_lo_16
<< CSL_SRIO_RIO_PF_16B_CNTL_DEVID_16B_LO_SHIFT);
gp_srioRegs->PF_CNTL[i].RIO_PF_8B_CNTL =
(PktForwardingEntry_cfg[i].forwardingID_up_8
<< CSL_SRIO_RIO_PF_8B_CNTL_DEVID_8B_UP_SHIFT)
|(PktForwardingEntry_cfg[i].forwardingID_lo_8
<< CSL_SRIO_RIO_PF_8B_CNTL_DEVID_8B_LO_SHIFT)
|(PktForwardingEntry_cfg[i].outport
<< CSL_SRIO_RIO_PF_8B_CNTL_OUT_PORT_SHIFT);
}
}
/*****************************************************************************
Prototype : KeyStone_SRIO_MulticastID_Cfg
Description : configure SRIO MulticastID
Input : SRIO_Multicast_ID_Cfg * multicastID
Uint32 uiNumMulticastID
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Brighton Feng
Modification : Created function
*****************************************************************************/
void KeyStone_SRIO_MulticastID_Cfg(
SRIO_Multicast_ID_Cfg * multicastID,
Uint32 uiNumMulticastID)
{
int i = 0;
uiNumMulticastID= _min2(SRIO_MAX_MULTICAST_ID_NUM, uiNumMulticastID);
for(i=0; i<uiNumMulticastID; i++)
{
gp_srioRegs->RIO_MULTIID_REG[i] =
(multicastID[i].multicast_8b_ID
<< CSL_SRIO_RIO_MULTIID_REG_16B_NODEID_SHIFT)
|(multicastID[i].multicast_8b_ID
<< CSL_SRIO_RIO_MULTIID_REG_8B_NODEID_SHIFT);
}
}
/*****************************************************************************
Prototype : KeyStone_SRIO_Flow_Control
Description : SRIO flow control setup
Input : SRIO_Flow_Control_ID * flowControlID
Uint32 uiNumFlowControlID
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Brighton Feng
Modification : Created function
*****************************************************************************/
void KeyStone_SRIO_Flow_Control(
SRIO_Flow_Control_ID * flowControlID,
Uint32 uiNumFlowControlID)
{
int i;
Uint32 uiFlowMask = 0;
if(NULL != flowControlID)
{
uiNumFlowControlID= _min2(14, uiNumFlowControlID);
for(i= 0; i< uiNumFlowControlID; i++)
gp_srioRegs->RIO_FLOW_CNTL[i]=
(flowControlID[i].tt<<CSL_SRIO_RIO_FLOW_CNTL_TT_SHIFT)
|flowControlID[i].flow_control_ID;
uiFlowMask= _set(uiFlowMask, 0, uiNumFlowControlID-1);
uiFlowMask= _pack2(uiFlowMask, uiFlowMask);
/*enable flow control in all TX modules*/
for(i= 0; i< SRIO_MAX_LSU_NUM/2; i++)
gp_srioRegs->RIO_LSU_FLOW_MASKS[i]= uiFlowMask;
for(i= 0; i< SRIO_PKTDMA_MAX_CH_NUM/2; i++)
gp_srioRegs->RIO_TX_CPPI_FLOW_MASKS[i]= uiFlowMask;
}
}
/*****************************************************************************
Prototype : KeyStone_SRIO_Prioirity_Permission_Setup
Description : Priority setup
Input : SRIO_priority_permission * priority_permission
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Brighton Feng
Modification : Created function
*****************************************************************************/
void KeyStone_SRIO_Prioirity_Permission_Setup(
SRIO_priority_permission * priority_permission)
{
if(NULL != priority_permission)
{
gp_srioRegs->RIO_PER_SET_CNTL = (gp_srioRegs->RIO_PER_SET_CNTL
&(~(CSL_SRIO_RIO_PER_SET_CNTL_CBA_TRANS_PRI_MASK))) /*clear the field*/
|(priority_permission->uiVbusPriority
<<CSL_SRIO_RIO_PER_SET_CNTL_CBA_TRANS_PRI_SHIFT);
gp_srioRegs->RIO_SUPERVISOR_ID =
(priority_permission->supervisorHostID_8b<<
CSL_SRIO_RIO_SUPERVISOR_ID_8B_SUPRVSR_ID_SHIFT)
|(priority_permission->supervisorHostID_16b<<
CSL_SRIO_RIO_SUPERVISOR_ID_16B_SUPRVSR_ID_SHIFT);
}
}
/*****************************************************************************
Prototype : KeyStone_SRIO_Interrupt_init
Description : SRIO interrupt configuration
Input : SRIO_Interrupt_Cfg * interrupt_cfg
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Brighton Feng
Modification : Created function
*****************************************************************************/
void KeyStone_SRIO_Interrupt_init(
SRIO_Interrupt_Cfg * interrupt_cfg)
{
Uint32 i;
Uint32 reg, shift;
volatile Uint32 * ICRR= (volatile Uint32 *)gp_srioRegs->DOORBELL_ICRR;
if(NULL == interrupt_cfg)
return;
/* Clear all the interrupts */
for(i=0; i<2; i++)
{
gp_srioRegs->LSU_ICSR_ICCR[i].RIO_LSU_ICCR = 0xFFFFFFFF ;
}
for(i=0; i<4; i++)
{
gp_srioRegs->DOORBELL_ICSR_ICCR[i].RIO_DOORBELL_ICCR = 0xFFFFFFFF;
}
gp_srioRegs->RIO_ERR_RST_EVNT_ICCR = 0xFFFFFFFF;
if(NULL != interrupt_cfg->interrupt_map)
{
for(i=0; i<interrupt_cfg->uiNumInterruptMap; i++)
{
/* Get register index for the interrupt source*/
reg = interrupt_cfg->interrupt_map[i].interrupt_event >> 16;
/* Get shift value for the interrupt source*/
shift = interrupt_cfg->interrupt_map[i].interrupt_event & 0x0000FFFF;
ICRR[reg]= (ICRR[reg]&(~(0xF<<shift))) /*clear the field*/
|(interrupt_cfg->interrupt_map[i].INTDST_number<<shift);
}
}
gp_srioRegs->RIO_INTERRUPT_CTL = interrupt_cfg->doorbell_route_ctl;
/*disable interrupt rate control*/
gp_srioRegs->RIO_INTDST_RATE_DIS= 0xFFFF;
for(i= 0; i< 16; i++)
{
gp_srioRegs->RIO_INTDST_RATE_CNT[i]= 0;
}
if(NULL != interrupt_cfg->interrupt_rate)
{
/*setup interrupt rate for specific INTDST*/
for(i= 0; i<interrupt_cfg->uiNumInterruptRateCfg; i++)
{
/*enable rate control for this INTDST*/
gp_srioRegs->RIO_INTDST_RATE_DIS &=
~(1<<interrupt_cfg->interrupt_rate[i].INTDST_number);
/*set interrupt rate counter for this INTDST*/
gp_srioRegs->RIO_INTDST_RATE_CNT[i]=
interrupt_cfg->interrupt_rate[i].interrupt_rate_counter;
}
}
for(i=0;i<32;i++)
CSL_SRIO_RouteLSUInterrupts(gp_srioRegs, i, 0);
return;
}
/*****************************************************************************
Prototype : KeyStone_SRIO_Timeout_Config
Description : SRIO timeout configuration in microsecond
Input : SRIO_Config * srio_cfg
Uint32 logicalRepsonseTimeout_us
Uint32 physicalPortTimeout_us
Uint32 linkInitSilenceTimeout_us
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Brighton Feng
Modification : Created function
*****************************************************************************/
void KeyStone_SRIO_Timeout_Config(SRIO_Config * srio_cfg,
Uint32 logicalRepsonseTimeout_us,
Uint32 physicalPortTimeout_us,
Uint32 linkInitSilenceTimeout_us)
{
Uint32 uiTimeout, uiMaxTimeout;
Uint32 byteClockMHz;
/*PRESCALAR_SELECT is used to divide VBUSM clock(normally 333 to 400MHz,
here use 350MHz), (VBUS_M clock)/(PRESCALAR_SELECT+1),
to get about 50MHz clock with about 20ns period.*/
gp_srioRegs->RIO_PER_SET_CNTL= (gp_srioRegs->RIO_PER_SET_CNTL
&(~CSL_SRIO_RIO_PER_SET_CNTL_PRESCALER_SELECT_MASK))
|((350/50-1)<<CSL_SRIO_RIO_PER_SET_CNTL_PRESCALER_SELECT_SHIFT);
// |((gDSP_Core_Speed_Hz/1000000/3/50-1)<<CSL_SRIO_RIO_PER_SET_CNTL_PRESCALER_SELECT_SHIFT);
/*logical layer response timeout
logicalRepsonseTimeout = 15 x (scaled VBUS_M clock period) x TIMEOUT_VALUE),
TIMEOUT_VALUE = logicalRepsonseTimeout/(scaled VBUS_M clock period)/15 */
uiTimeout= logicalRepsonseTimeout_us*1000/20/15;
uiMaxTimeout=CSL_SRIO_RIO_SP_RT_CTL_TVAL_MASK
>>CSL_SRIO_RIO_SP_RT_CTL_TVAL_SHIFT;
if(uiTimeout>uiMaxTimeout)
uiTimeout= uiMaxTimeout;
if(0==uiTimeout)
uiTimeout= 1;
gp_srioRegs->RIO_SP_RT_CTL= uiTimeout<<CSL_SRIO_RIO_SP_RT_CTL_TVAL_SHIFT;
/*SRV_CLK should be scaled to about 10MHz (about 100ns period).
SRV_CLK= (a SRIO internal IP clock)/ PRESCALAR_SRV_CLK.
The SRIO internal IP clock is the byte clock of
one of the lanes (selected by SYS_CLK_SEL).
(Byte clock) = (link rate)/20.*/
gp_srioRegs->RIO_PRESCALAR_SRV_CLK=
(Uint32)srio_cfg->serdes_cfg->commonSetup.inputRefClock_MHz/10;
/*physical layer response timeout.
physicalPortTimeout = SRV_CLK period * TIMEOUT_VALUE * 3,
TIMEOUT_VALUE = physicalPortTimeout/SRV_CLK period/3 */
uiTimeout= physicalPortTimeout_us*1000/100/3;
uiMaxTimeout=CSL_SRIO_RIO_SP_LT_CTL_TVAL_MASK
>>CSL_SRIO_RIO_SP_LT_CTL_TVAL_SHIFT;
if(uiTimeout>uiMaxTimeout)
uiTimeout= uiMaxTimeout;
if(0==uiTimeout)
uiTimeout= 1;
gp_srioRegs->RIO_SP_LT_CTL= uiTimeout<<CSL_SRIO_RIO_SP_LT_CTL_TVAL_SHIFT;
/*port silence timeout
The SRIO starts in the SILENT state. The link output driver is disabled
to force the link partner to initialize regardless of its current state.
The duration of the SILENT state is controlled by the silence_timer.
The duration must be long enough to ensure that the link partner detects
the silence (as a loss of lane_sync) and is forced to initialize but short
enough that it is readily distinguished from a link break.
linkInitSilenceTimeout is SRV_CLK period X 410 X SILENCE_TIMER,
SILENCE_TIMER= linkInitSilenceTimeout/SRV_CLK period/410*/
uiTimeout= linkInitSilenceTimeout_us*1000/100/410;
uiMaxTimeout=CSL_SRIO_RIO_PLM_SP_SILENCE_TIMER_SILENCE_TIMER_MASK
>>CSL_SRIO_RIO_PLM_SP_SILENCE_TIMER_SILENCE_TIMER_SHIFT;
if(uiTimeout>uiMaxTimeout)
uiTimeout= uiMaxTimeout;
if(0==uiTimeout)
uiTimeout= 1;
uiTimeout= uiTimeout
<<CSL_SRIO_RIO_PLM_SP_SILENCE_TIMER_SILENCE_TIMER_SHIFT;
if(srio_cfg->blockEn.bLogic_Port_EN[0])
gp_srioRegs->RIO_PLM[0].RIO_PLM_SP_SILENCE_TIMER= uiTimeout;
if(srio_cfg->blockEn.bLogic_Port_EN[1])
gp_srioRegs->RIO_PLM[1].RIO_PLM_SP_SILENCE_TIMER= uiTimeout;
if(srio_cfg->blockEn.bLogic_Port_EN[2])
gp_srioRegs->RIO_PLM[2].RIO_PLM_SP_SILENCE_TIMER= uiTimeout;
if(srio_cfg->blockEn.bLogic_Port_EN[3])
gp_srioRegs->RIO_PLM[3].RIO_PLM_SP_SILENCE_TIMER= uiTimeout;
}
Bool SrioWaitPllToLock(long long timeover)
{
long long totalTime;
totalTime = timeover;
if(DRIVER_WAIT_FOREVER == timeover)
{
while(1)
{
if((boot_cfg_regs->STS_SRIO & 0x00000001) == 0x00000001)
break;
else
tsc_delay_us(1);
}
}
else
{
while(1)
{
if(((boot_cfg_regs->STS_SRIO & 0x00000001) == 0x00000001)
|| totalTime < 0)
break;
else
{
tsc_delay_us(1);
totalTime -= 1000;
}
}
}
if(totalTime<0)
return FALSE;
else
return TRUE;
}
Bool SrioWaitPortToLink(int port,long long timeover)
{
long long totalTime;
totalTime = timeover;
if(DRIVER_WAIT_FOREVER == timeover)
{
while(1)
{
if(0!=(gp_srioRegs->RIO_SP[port].RIO_SP_ERR_STAT&
CSL_SRIO_RIO_SP_ERR_STAT_PORT_OK_MASK))
break;
else
tsc_delay_us(1);
}
}
else
{
while(1)
{
if(0!=(gp_srioRegs->RIO_SP[port].RIO_SP_ERR_STAT&
CSL_SRIO_RIO_SP_ERR_STAT_PORT_OK_MASK)|| totalTime < 0)
break;
else
{
tsc_delay_us(1);
totalTime -= 1000;
}
}
}
if(totalTime<0)
return FALSE;
else
return TRUE;
}
int SrioGetLinkWidth(int port)
{
Uint8 regVal;
CSL_SRIO_GetInitializedPortWidth(gp_srioRegs, port, ®Val);
if((0 == regVal) || (1 == regVal))
return 1;
else if(2 == regVal)
return 4;
else
return 0;
}
void SrioFirstTestCode(void)
{
gp_srioRegs->RIO_PER_SET_CNTL = 0x01053800;
gp_srioRegs->BLOCK_ENABLE_STATUS[3].RIO_BLK_EN = 1;
gp_srioRegs->BLOCK_ENABLE_STATUS[4].RIO_BLK_EN = 1;
gp_srioRegs->RIO_INTDST_RATE_DIS=1;
gp_srioRegs->RIO_PE_FEAT = 0x20000199;
gp_srioRegs->RIO_SP[0].RIO_SP_LM_RESP = 0;
gp_srioRegs->RIO_SP[0].RIO_SP_CTL2 = 0x02AA0000;
gp_srioRegs->RIO_SP[0].RIO_SP_CTL = 0xD0600001;
gp_srioRegs->RIO_SP[1].RIO_SP_CTL = 0x600001;
gp_srioRegs->RIO_SP[2].RIO_SP_CTL = 0x600001;
gp_srioRegs->RIO_SP[3].RIO_SP_CTL = 0x600001;
gp_srioRegs->RIO_SP_ERR[0].RIO_SP_RATE_EN = 0;
gp_srioRegs->RIO_SP_ERR[0].RIO_SP_ERR_ATTR_CAPT = 0;
gp_srioRegs->RIO_SP_ERR[0].RIO_SP_ERR_THRESH = 0;
gp_srioRegs->RIO_LANE[0].RIO_LANE_STAT0 = 0x7f88;
gp_srioRegs->RIO_LANE[1].RIO_LANE_STAT0 = 0x107f88;
gp_srioRegs->RIO_LANE[3].RIO_LANE_STAT0 = 0x307f88;
gp_srioRegs->RIO_PLM[0].RIO_PLM_SP_ALL_PW_EN = 1;
gp_srioRegs->RIO_PLM[0].RIO_PLM_SP_DISCOVERY_TIMER = 0x20000000;
}
void SrioSecondTestCode(void)
{
int i,j;
for(i=0;i<0x10000;i++);
for(j=0;j<5;j++)
{
for(i=0; i<SRIO_MAX_PORT_NUM; i++)
{
gp_srioRegs->RIO_SP_ERR[i].RIO_SP_ERR_DET = 0;
gp_srioRegs->RIO_SP[i].RIO_SP_ERR_STAT = 0xfffffff0;
gp_srioRegs->RIO_PLM[i].RIO_PLM_SP_LONG_CS_TX1 = 0x2003F044;
}
for(i=0;i<0x1000;i++);
}
}
/*****************************************************************************
Prototype : KeyStone_SRIO_Init
Description : SRIO initialization
Input : SRIO_Config * srio_cfg
Output : None
Return Value :
History :
1.Date : 2011/6/11
Author : Brighton Feng
Modification : Created function
2.Date : 2011/6/13
Author : Zhan
Modification : Modify the LSU setup and SERDES configuration
*****************************************************************************/
int KeyStone_Srio_Init(SRIO_Config* srio_cfg, long long timeover)
{
Uint32 cfgValue = 0;
Uint32 i = 0;
/* Route LSU0 ICR0 to INTDST0 */
CSL_SRIO_RouteLSUInterrupts(gp_srioRegs, 0, 0);
/* Route LSU1 ICR0 to INTDST0 */
CSL_SRIO_RouteLSUInterrupts(gp_srioRegs, 1, 0);
/* Route LSU2 ICR0 to INTDST0 */
CSL_SRIO_RouteLSUInterrupts(gp_srioRegs, 2, 0);
//enable SRIO power and clock domain
KeyStone_enable_PSC_module(CSL_PSC_PD_SRIO, CSL_PSC_LPSC_SRIO);
/*Clear BOOT_COMPLETE bit*/
gp_srioRegs->RIO_PER_SET_CNTL &= (~(1 << CSL_SRIO_RIO_PER_SET_CNTL_BOOT_COMPLETE_SHIFT));
//bring SRIO from reset isolation
gp_srioRegs->RIO_PCR = 0x11;
/*enable globally used blocks including MMR block in SRIO*/
KeyStone_SRIO_GlobalEnable();
/*The LSU setup registers are only programmable
while the LSU is disabled while the peripheral is enabled.*/
if(srio_cfg->lsu_cfg)
{
/*setup the shadow registers allocation between LSU*/
gp_srioRegs->RIO_LSU_SETUP_REG0 =
(srio_cfg->lsu_cfg->lsuGrp0ShadowRegsSetup << CSL_SRIO_RIO_LSU_SETUP_REG0_SHADOW_GRP0_SHIFT)|
(srio_cfg->lsu_cfg->lsuGrp1ShadowRegsSetup << CSL_SRIO_RIO_LSU_SETUP_REG0_SHADOW_GRP1_SHIFT);
/*setup LSU interrupt based on LSU number or Source ID*/
cfgValue = 0;
for(i=0; i<SRIO_MAX_LSU_NUM; i++)
{
cfgValue |= srio_cfg->lsu_cfg->lsuIntSetup[i] << i;
}
gp_srioRegs->RIO_LSU_SETUP_REG1 = cfgValue;
}
/*enable other optional blocks*/
KeyStone_SRIO_enable_blocks(&srio_cfg->blockEn);
if(SRIO_SERDES_LOOPBACK==srio_cfg->loopback_mode)
{
if(srio_cfg->serdes_cfg->linkSetup[0])
srio_cfg->serdes_cfg->linkSetup[0]->loopBack = SERDES_LOOPBACK_ENABLE;
if(srio_cfg->serdes_cfg->linkSetup[1])
srio_cfg->serdes_cfg->linkSetup[1]->loopBack = SERDES_LOOPBACK_ENABLE;
if(srio_cfg->serdes_cfg->linkSetup[2])
srio_cfg->serdes_cfg->linkSetup[2]->loopBack = SERDES_LOOPBACK_ENABLE;
if(srio_cfg->serdes_cfg->linkSetup[3])
srio_cfg->serdes_cfg->linkSetup[3]->loopBack = SERDES_LOOPBACK_ENABLE;
}
SRIO_HyperLink_Serdes_init(srio_cfg->serdes_cfg, gp_srioSerdesRegs);
if(!SrioWaitPllToLock(timeover))
return DRIVER_RESULT_PLL_UNLOCK;
KeyStone_SRIO_set_1x2x4x_Path(srio_cfg->srio_1x2x4x_path_control);
KeyStone_SRIO_set_device_ID(srio_cfg->device_ID_routing_config,
srio_cfg->uiNumDeviceId);
KeyStone_SRIO_CSR_CAR_Config(srio_cfg);
/*Allocates ingress Data Nodes and Tags based on priority.
These registers must only be changed while boot_complete is
deasserted or while the port is held in reset.*/
for(i=0;i<SRIO_MAX_PORT_NUM;i++)
{
if(FALSE == srio_cfg->blockEn.bBLK5_8_Port_Datapath_EN[i])
continue;
/*maximum data nodes and tags are 72 (0x48).
Each data node stores 32 bytes of data*/
gp_srioRegs->RIO_PBM[i].RIO_PBM_SP_IG_WATERMARK0 =
(36<<CSL_SRIO_RIO_PBM_SP_IG_WATERMARK0_PRIO0_WM_SHIFT)
|(32<<CSL_SRIO_RIO_PBM_SP_IG_WATERMARK0_PRIO0CRF_WM_SHIFT);
gp_srioRegs->RIO_PBM[i].RIO_PBM_SP_IG_WATERMARK1 =
(28<<CSL_SRIO_RIO_PBM_SP_IG_WATERMARK1_PRIO1_WM_SHIFT)
|(24<<CSL_SRIO_RIO_PBM_SP_IG_WATERMARK1_PRIO1CRF_WM_SHIFT);
gp_srioRegs->RIO_PBM[i].RIO_PBM_SP_IG_WATERMARK2 =
(20<<CSL_SRIO_RIO_PBM_SP_IG_WATERMARK2_PRIO2_WM_SHIFT)
|(16<<CSL_SRIO_RIO_PBM_SP_IG_WATERMARK2_PRIO2CRF_WM_SHIFT);
gp_srioRegs->RIO_PBM[i].RIO_PBM_SP_IG_WATERMARK3 =
(12<<CSL_SRIO_RIO_PBM_SP_IG_WATERMARK3_PRIO3_WM_SHIFT)
|(8<<CSL_SRIO_RIO_PBM_SP_IG_WATERMARK3_PRIO3CRF_WM_SHIFT);
}
/*setup timeout value in microsecond*/
KeyStone_SRIO_Timeout_Config(srio_cfg, 500000, 50, 100);
KeyStone_SRIO_RxMode_Setup(srio_cfg->rxMode);
KeyStone_SRIO_packet_forwarding_Cfg(srio_cfg->PktForwardingEntry_cfg,
srio_cfg->uiNumPktForwardingEntry);
KeyStone_SRIO_MulticastID_Cfg(srio_cfg->multicastID,
srio_cfg->uiNumMulticastID);
KeyStone_SRIO_Flow_Control(srio_cfg->flowControlID,
srio_cfg->uiNumFlowControlID);
KeyStone_SRIO_Prioirity_Permission_Setup(
srio_cfg->priority_permission);
KeyStone_SRIO_Interrupt_init(srio_cfg->interrupt_cfg);
if(SRIO_DIGITAL_LOOPBACK==srio_cfg->loopback_mode)
{
gp_srioRegs->RIO_PER_SET_CNTL1 |=
(0xF<<CSL_SRIO_RIO_PER_SET_CNTL1_LOOPBACK_SHIFT);
}
else if(SRIO_EXTERNAL_LINE_LOOPBACK==srio_cfg->loopback_mode)
{
for(i=0; i<SRIO_MAX_PORT_NUM; i++)
{
gp_srioRegs->RIO_PLM[i].RIO_PLM_SP_IMP_SPEC_CTL=
(1<<CSL_SRIO_RIO_PLM_SP_IMP_SPEC_CTL_LLB_EN_SHIFT);
}
}
/*Set BOOT_COMPLETE bit*/
gp_srioRegs->RIO_PER_SET_CNTL |= (1 << CSL_SRIO_RIO_PER_SET_CNTL_BOOT_COMPLETE_SHIFT);
/*This should be the last enable bit to toggle when bringing the
device out of reset to begin normal operation.*/
gp_srioRegs->RIO_PCR|= CSL_SRIO_RIO_PCR_PEREN_MASK;
SrioFirstTestCode();
for(i=0; i<SRIO_MAX_PORT_NUM; i++)
{
if(srio_cfg->blockEn.bLogic_Port_EN[i])
{
if(!SrioWaitPortToLink(i,timeover))
return DRIVER_RESULT_LINK_TIMEOUT;
}
}
int linkWidth = 0;
if(SRIO_PATH_CTL_4xLaneABCD == srio_cfg->srio_1x2x4x_path_control)
{
linkWidth = SrioGetLinkWidth(0);
if(4 != linkWidth)
return DRIVER_LINK_STAT_ERROR;
}
//for debug
KeyStone_SRIO_Error_Capture_Enable(&srio_cfg->blockEn);
SrioSecondTestCode();
return DRIVER_RESULT_OK;
}