This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSL library MMC_Init function is setting both serial ports by default



Hello,

I noticed that in the MMC_Init function following happens:

/* Enable Serial port 0 pin for mmcsd0  */

CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_SP0MODE, MODE0);

/* Enable Serial port 1 pin for mmcsd1  */

CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_SP1MODE, MODE0);

EBSR is set to enable mmcsd0 and mmcsd1. Since I only use mmcsd0 and have other stuff on port #2 I have to call MMC_Init() and then reset the EBSR register in the code manually after that. This seams illogical to me (and looks ugly in the code)  and prone to errors. I had trouble figuring out what was wrong with my code until I realized that this function is messing up the registers.  I would suggest to parametrize the function to accept which port should be initialized. For example:

MMC_Init (MMC_SD0);

Cheers,