I work with am5728-evm and I want to test wireless connection.
root@am57xx-evm:~# ifconfig
eth0 Link encap:Ethernet HWaddr 5C:F8:21:0E:96:28
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:107
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:263 errors:0 dropped:0 overruns:0 frame:0
TX packets:263 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:271702 (265.3 KiB) TX bytes:271702 (265.3 KiB)
wlan0 Link encap:Ethernet HWaddr E0:E5:CF:9B:51:B1
inet addr:192.168.0.24 Bcast:0.0.0.0 Mask:255.255.255.255
inet6 addr: fe80::e2e5:cfff:fe9b:51b1/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:1540 errors:0 dropped:0 overruns:0 frame:0
TX packets:132 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:137179 (133.9 KiB) TX bytes:14478 (14.1 KiB)
root@am57xx-evm:~# iw dev wlan0 link
Connected to 78:54:2e:89:08:a1 (on wlan0)
SSID: D-Link_DIR-600
freq: 2412
RX: 101614 bytes (932 packets)
TX: 6672 bytes (88 packets)
signal: -50 dBm
tx bitrate: 72.2 MBit/s MCS 7 short GI
bss flags: short-slot-time
dtim period: 1
beacon int: 100
root@am57xx-evm:~#
I use "ping www.google.com" but I encounter the following error:
root@am57xx-evm:~# ping www.google.com
ping: bad address 'www.google.com'
root@am57xx-evm:~#