This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Davince and Linux

Hi

Is it correct that there are two versions of Linux available for the Davince processors?

A- Montavista

B- open source Linus (ubuntu?)

And where does GStreamer fits in?

thanks.

  • Which DaVinci Device (DM6446, DM355, DM6437, DM6467, DM365...) are you working with?

    In most cases, you should have a combination of the following: 1) demo montavista version, 2) professional montavista version and 3) GIT open source kernel. 

    The idea is to have a free version of kernel (option 1 or 3 above) and a professional distro (option 2) above for our customers to have access to.  Based on customer feedback, we are moving from option 1 to option 3 on all our new products as well as slowly migrating out legacy products to option 3 for the free kernel.  Hence you should always have a free version of the kernel available for our devices; during this transitionary period, you may have both option 1 and 3 available for some devices.

    I am not sure if Ubuntu is a good fit in the embedded space; it is likely a better host Linux OS for your host PC than a target embdded OS.  The three options above are from a target Linux Kernel perspective.