This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to convert and edit HD video: TS, MTS, M2TS

This article provides two parts will show you how to convert and edit HD video such as HD TS, HD MTS, HD M2TS, HD MPEG, HD WMV, HD MPG, HD MP4, QuickTime HD MOV, HD H.264, HD RM video, etc.

Part One: How to convert HD video
Part Two: How to edit HD video

Part One: How to convert Hd video

Tools Introduction:
Aiseesoft HD Video Converter is best HD Converter to convert HD TS, HD MTS, HD M2TS, HD MPEG, HD WMV, HD MPG, HD MP4, QuickTime HD MOV, HD H.264, HD RM video, etc.

Quick Guide:
Step 1: Download HD Video Converter
Download the HD Video Converter, then install and run this program.

Step 2: Load the HD video files you want to convert
Click the "Add File" button to browse your computer hard disc and add the HD video files you want to convert to the program.

Step 3: Output Settings
After you added HD Video files, you can select an output format for each video file and specify a directory on your computer to save the output files.

Aiseesoft HD Video Converter supports comprehensive video formats including MPEG-4, H.264/MPEG-4 AVC, MOV, M4V, AVI, DivX, XviD, ASF, WMV, MPEG-1, MPEG-2, 3GP, 3GPP, MKV, FLV, SWF, VOB, DV, Super VCD (NTSC, PAL, SECAM), VCD(NTSC, PAL, SECAM) , DVD(NTSC, PAL, SECAM).
If you don't know what formats your device supports, you can just select the format according to the device name. For exapmle, you can select ' iPod Video MPEG-4(*.mp4)' when you want to convert HD video to iPod Video. The default setting works well. Of course, if you don't want to use the default video and audio encoding settings, just click the "Settings" button to customize these settings.

Step 4: Start the conversion
Click the Convert button to start conversion and then you can just go out for a walk or take a nap, and the conversion may have been finished when you come back: )

Part Two: How to edit HD video

1. Adjust Effect
Click "Effect" button to open the edit window to adjust the video effects.

Brightness: Drag the Brightness adjustment bar to set the brightness of the video.
Contrast: Drag the Contrast adjustment bar to set the contrast of the video.
Saturation: Drag the Saturation adjustment bar to set the saturation of the video.
Volume: Drag the Volume adjustment bar to adjust the volume of the audio.

2. Trim video clips
Click "Trim"button to open the edit window to trim any video clips.

3. Crop video play ragion
Click "Crop" button to open the edit window to customize the video play region.

Done.

  • I am using Pavtube HD Video Converter ,it allows you to edit and convert HD video formats from HD camcorders, TiVo DVRs or DVs (like JVC, Panasonic, and Cannon) to other formats including MP4, 3GP, AVI, MPG, MPEG-4, FLV, MOV, 3G2, VOB, MP3, FLAC, MKA, OGG, WAV, AC3, M4A etc. so that you can enjoy the HD videos on portable devices like iPod, iPhone, iPhone 3G cell phones, Apple TV, PSP, BlackBerry, Creative Zen, iriver, Zune, etc. on the go.you can have a try ,here is the link ; http://www.pavtube.com/hd-video-converter