Other Parts Discussed in Thread: OMAPL138, AM1705, AM1808, AM1707, AM1806, SYSBIOS, OMAP-L138, MATHLIB
Tool/software: Linux
Hi there I have installed the SDK 4.0.0.4 for Linux and it did install /opt/ti/ipc_3_46_00_02
I have made changes to products.mak and would like to build examples designs for OMAPL138
hence set the PLATFORM=OMAPL138
got the following error after running
sudo make -f ipc-bios.mak all
...Build of libraries done.
cle674 package/cfg/bin/ti_platforms_evmOMAPL138_DSP/nano_test_pe674.c ...
======== .dlls [./packages/ti/ipc/transports/] ========
======== .dlls [./packages/ti/pm/] ========
======== .dlls [./packages/ti/sdo/ipc/] ========
configuring instrumented.pe9 from package/cfg/instrumented_pe9.cfg ...
The TMS470R10 device is not currently supported.
The following devices are supported in the ti.catalog.arm catalog:
AM1705 AM1707 AM1806 AM1808 CortexM3
OMAPL108 OMAPL118 OMAPL137 OMAPL138 TMS320CDM730
TMS320CDM740 TMS320DA805 TMS320DA807 TMS320DA808 TMS320DA810
TMS320DA828 TMS320DA830 TMS320DA840 TMS320DA850
js: "/opt/ti/bios_6_46_05_55/packages/ti/sysbios/family/arm/Settings.xs", line 613: Error: Unsupported device!
"/opt/ti/bios_6_46_05_55/packages/ti/sysbios/family/arm/Settings.xs", line 772
"/opt/ti/bios_6_46_05_55/packages/ti/sysbios/family/Settings.xs", line 241
"/opt/ti/bios_6_46_05_55/packages/ti/sysbios/family/Settings.xs", line 120
"./package/cfg/instrumented_pe9.cfg", line 185
gmake[1]: *** [package/cfg/instrumented_pe9.xdl] Error 1
gmake: *** [packages/ti/sdo/ipc/,.dlls] Error 2
ipc-bios.mak:138: recipe for target 'all' failed
make: *** [all] Error 2