This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320VC5416: TMS320VC5416 boot problem

Part Number: TMS320VC5416

Tool/software: Code Composer Studio

Hello guys,

I have to download a .out file into my TMS320VC5416 DSP.

I'm using:

- Code Compeser Studio 5.5

- Emulator Olimex XDS100V3

- Emulator SW pack

I successfully tested the connection to my emulator, I can connect the target, I can do "Load Program" and correctly run the file, but I loose it when I switch off my board.

The .out file contains also the boot inside.

Can anyone help me?

Thanks in advance,

Alfredo