Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Tool/software: Starterware
Why My Board Not Erased ?
D:\Work\OMAPL138_StarterWare_1_10_04_01_21092017Work\ARMDSPTestWit
Change_300Mhz>sfh_OMAP-L138.exe -targettype OMAPL138_LCDK -flashty
7 -erase
-----------------------------------------------------
TI Serial Flasher Host Program for OMAP-L138
(C) 2011, Texas Instruments, Inc.
Ver. 1.67
-----------------------------------------------------
[TYPE] Global erase
[TARGET] OMAPL138_LCDK
[DEVICE] NAND
[NAND Block] 1
Attempting to connect to device COM7...
Press any key to end this program at any time.
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Waiting for BOOTME... (power on or reset target now)
(AIS Parse): BOOTME received!
(AIS Parse): Performing Start-Word Sync...
(AIS Parse): Performing Ping Opcode Sync...
(AIS Parse): Processing command 0: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 13500-Byte section to address 0x80000000.
(AIS Parse): Processing command 1: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 1440-Byte section to address 0x800034BC.
(AIS Parse): Processing command 2: 0x58535906.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Performing jump and close...
(AIS Parse): AIS complete. Jump to address 0x80000000.
(AIS Parse): Waiting for DONE...
(AIS Parse): Boot completed successfully.
Waiting for SFT on the OMAP-L138...