Other Parts Discussed in Thread: ADS1118
Tool/software: Linux
Hello.
I noticed that I can't longer wake up my device from standby by using a GPIO after upgrading to the v4.9 Kernel.
According to the link below it shouldn't require special configuration. I'm using a gpio3, which is on the first bank (which AFAIK is the only bank allowed to wakeup, even though the documentation doesn't mention it):
http://processors.wiki.ti.com/index.php/AM335x_Power_Management_Standby_User%27s_Guide#GPIO_wakeup
Both devices have the same config on debugfs:
root@dev:~# cat /sys/kernel/debug/gpio
gpiochip0: GPIOs 0-31, parent: platform/44e07000.gpio, gpio:
gpio-2 ( |sysfs ) in lo IRQ
gpio-3 ( |sysfs ) in lo IRQ
gpio-6 ( |sysfs ) out lo
gpio-8 ( |? ) out lo
gpio-9 ( |? ) out hi
gpio-13 ( |omap-serial ) out lo
gpio-29 ( |reset ) out hi
gpiochip1: GPIOs 32-63, parent: platform/4804c000.gpio, gpio:
gpiochip2: GPIOs 64-95, parent: platform/481ac000.gpio, gpio:
gpio-64 ( |sysfs ) out lo
gpio-70 ( |ASD1118 /En 20mA 1 ) out lo
gpio-71 ( |ASD1118 /En 10V 3 ) out hi
gpio-72 ( |ASD1118 /En 20mA 3 ) out lo
gpio-73 ( |ASD1118 /En 20mA 4 ) out lo
gpio-74 ( |ASD1118 /En 10V 4 ) out hi
gpio-75 ( |ASD1118 /En 20mA 2 ) out lo
gpio-76 ( |ASD1118 /En 10V 2 ) out hi
gpio-77 ( |ASD1118 /En 10V 1 ) out hi
gpio-80 ( |ASD1118 /En PT100 3 ) out lo
gpio-81 ( |ASD1118 /En PT100 1 ) out lo
gpio-89 ( |sysfs ) in lo
gpio-90 ( |the-button ) in hi IRQ
gpiochip3: GPIOs 96-127, parent: platform/481ae000.gpio, gpio:
gpio-114 ( |data-gpio ) out lo
gpio-115 ( |rclk-gpio ) out lo
gpio-116 ( |srclk-gpio ) out lo
gpiochip5: GPIOs 502-509, parent: platform/shiftreg@0, shiftreg@0:
gpio-502 ( |? ) out lo
gpio-503 ( |? ) out lo
gpio-504 ( |? ) out lo
gpio-505 ( |? ) out lo
gpio-506 ( |? ) out lo
gpio-507 ( |? ) out lo
gpio-508 ( |? ) out lo
gpio-509 ( |? ) out lo
gpiochip4: GPIOs 510-511, parent: platform/50000000.gpmc, omap-gpmc:
How can I start debugging this?