This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TMS320C6455: can't find c6455 gel file

Part Number: TMS320C6455


Tool/software: TI-RTOS

Hi,all:
Where to find c6455 gel file? I didn't find it in the ccs_base folder.Where can I get it ?

  • Have you checked:
    /ti/ccsv7/ccs_base/emulation/boards/evmc6657l/gel

    Best Regards,
    Yordan
  • Hi,

    Is 6657l gel file the same with 6455 gel file ? In the ccs_base folder, I can't find evm6455 folder, but I can find dsk6455 folder, and in it I can find DSK6455.gel and DSK6455_Mezzanine.gel . When I generate a HELLO example in CCS v5, and import the DSK6455.gel in the project , errors show up as follow:

    C64XP_0: GEL Output: PLL1 has been configured.
    C64XP_0: 2: GEL StartUp Complete.
    C64XP_0: GEL Output: Turn off cache segment
    C64XP_0: GEL Output: Disable EDMA events
    IcePick_C_0: Error: (Error -154 @ 0x0) One of the FTDI driver functions used to write data returned bad status or an error. (Emulation package 5.1.232.0)
    IcePick_C_0: Unable to determine target status after 20 attempts
    IcePick_C_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
    C64XP_0: JTAG Communication Error: (Error -154 @ 0x0) One of the FTDI driver functions used to write data returned bad status or an error. (Emulation package 5.1.232.0)
    C64XP_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging

    why did this happen? when I test connection , it reported no  problem. 

  • Sorry, the devices are different.

    Can you check this thread:
    e2e.ti.com/.../310514

    Best Regards,
    Yordan
  • The GEL for this device is provided by the board manufacturer :
    c6000.spectrumdigital.com/.../