This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2E05: Uboot and Linux source code changes to match new clock frequency

Part Number: 66AK2E05


Hi,

We are designing a 66AK2E05 custom board and we are using PLL settings different from the EVM board.

The EVM board has following clock frequencies:

NETCPCLK : 100MHz

DDRCLK:100MHz

CORECLK:100MHz

SGMIICLK:156.25MHz

Whereas in our custom board, we have NETCPCLK: 125MHz and DDRCLK:125MHz; the CORECLK and SGMIICLK are the same. 

I am trying to change the EVM board's frequency to match our new clock frequencies through changing output of clock generator in the BMC. 

But, I wanted to know what changes should be done in U-boot and Linux source code to match these changed NETCPCLK and DDRCLK frequencies? I am using "ti-processor-sdk-linux-rt-k2e-evm-03.03.00.04" to build Uboot and Linux kernel images.

I am using UART bootmode once initially and then through TFTP, get a new Uboot image and burn to SPI flash and use SPI bootmode later on.

Can you please let me know the U-boot and Linux kernel source code changes needed to make the board boot up with these changed clock frequencies?

Regards,

Ashwini