Other Parts Discussed in Thread: OMAP-L137
We are new to OMAP L137.
We are purchasing spectrum digital OMAP-L137 floating point starter kit.
We want to know about the hardware and software tools that would be required for the development.
We would be using both the ARM and also the DSP cores of OMAP.
1) Would we be required to use Linux environment for the ARM core and CCS for the DSP core.
2) is there a way we can do the complete development for ARM & DSP using only the CCS tool.
If ( 2) is not possible than:
3) How do we download the binaries for ARM/DSP into the corresponding cores using the JTAG. Is there a way to combine both binaries and download as a single binary. In such cases how does the tool differentiate between DSP/ARM code sections
4) are there any in expensive linux tools for the ARM core?
5) if not could we use the monta vista environment that comes with OMAP starter kit also for development/production.
6) What are the limitation of this version of monta vista that comes with the OMAP starter kit ( code size? Time limit? Or function limit?)?
7) are all peripherals accessible from both ARM & DSP cores. If yes,why are USB and TCP/IP stacks available only for lInux?
8) From where can we get the drivers/stacks for the TCI/IP and USB of OMAP L1-37
9) where can we download demo examples?