I test the evm's af test program using a step motor lens.The modified program is below.
/////////////////////////////////////////////////////////////////////////////////////////////////
pace=0x8140//start motor position
while(pace<0x819d)
{
index=0;fv=0;
result = read(fd,(void *)buffer_stat,buff_size);
if(result < 0)
{
printf("\n Read Failed");
}
if(result >0)
{
//printf("\nOutput is in file af_samp.txt");
fprintf(fp1,"\npace=0x%x",pace);
k11= ( int *)buffer_stat;
for(count=0;count<buff_size/4;count++)
{
fprintf(fp1,"\n%d",k11[count]);
}
fv=k11[2];//use green fv value
fprintf(fp1,"\n%d",fv);
if(fv>fvmax)
{
fvmax=fv;
maxpace=pace;//record max fv value and step motor position
}
}
else
{
printf("\n *** NOT ABLE TO READ*****");
}
//printf("\n NO OF BYTES READ %d",result);
pace+=5;
//set to start focus position
setfocusposition(id232,pace);//step foward
//wait until reach the position
waitforreachsig(id232);//wait until motor stop
}
/////////////////////////////////////////////////////////////////////////////////////////////
I can't get a peak position using the green FV value.My paxel configuration is below:
/////////////////////////////////////////////////////////////////////////////////////////////////////////////////
struct af_configuration config;
int result = 0, index;
int iir0[12] = { 64, 0, 0, 21, 22, 21, 0, 0, -16, 32, -16 };
int iir1[12] = { 64, 0, 0, 21, 22, 21, 0, -29, -16, 32, -16 };
/*Open AF driver */
fd = open(DRIVER_NAME, O_RDWR);
if (fd < 0) {
printf("Error in opening AF Device\n");
return;
}
/* Select input source as SDRAM */
/* Enable Alaw */
config.alaw_enable = H3A_AF_ENABLE;
/*Set Horizontal Median filter*/
config.hmf_config.enable = H3A_AF_DISABLE;
config.hmf_config.threshold = 100;
/* Set paxel Parmateres */
config.iir_config.hz_start_pos = 2;
config.paxel_config.height = 32;
config.paxel_config.width = 124 ;
config.paxel_config.line_incr = 2;
config.paxel_config.vt_start = 60;
config.paxel_config.hz_start = 480;
config.paxel_config.hz_cnt = 1;
config.paxel_config.vt_cnt = 1;
/* Set Accumulator mode */
config.mode = ACCUMULATOR_SUMMED;
//config.mode = ACCUMULATOR_PEAK;
/* Set IIR Filter Parameters */
for (index = 0; index < 11; index++) {
config.iir_config.coeff_set0[index] = iir0[index];
config.iir_config.coeff_set1[index] = iir1[index];
}
/* Set RGBPOSITION */
config.rgb_pos = GR_BG_BAYER;
printf("\n Before SEt Params");
/* Call AF_S_PARAM to do the configuration */
buff_size = ioctl(fd,AF_S_PARAM,&config);