This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

mmcblk0boot1: unknown partition table

Hi All,

I am using Arm v7 Processor, After booting it is showing throwing this error message.

Jan 01 00:00:06 Docsis-Gateway kernel:  mmcblk0boot1: unknown partition table

Jan 01 00:00:06 Docsis-Gateway kernel:  mmcblk0boot0: unknown partition table

And the mounting of the kernel is shown,

Device         Boot     Start       End Blocks  Id System

/dev/mmcblk0p1             16     39103  19544  83 Linux

/dev/mmcblk0p2          39104     58687   9792  83 Linux

/dev/mmcblk0p3         106496   1011199 452352  83 Linux

Disk /dev/mmcblk0rpmb: 4 MiB, 4194304 bytes, 8192 sectors

Units: sectors of 1 * 512 = 512 bytes

Sector size (logical/physical): 512 bytes / 512 bytes

I/O size (minimum/optimal): 512 bytes / 512 bytes

 

Disk /dev/mmcblk0boot1: 4 MiB, 4194304 bytes, 8192 sectors

Units: sectors of 1 * 512 = 512 bytes

Sector size (logical/physical): 512 bytes / 512 bytes

I/O size (minimum/optimal): 512 bytes / 512 bytes

 

Disk /dev/mmcblk0boot0: 4 MiB, 4194304 bytes, 8192 sectors

Units: sectors of 1 * 512 = 512 bytes

Sector size (logical/physical): 512 bytes / 512 bytes

I/O size (minimum/optimal): 512 bytes / 512 bytes

Donot know what kind of warning message. please help me to resolve this issue.

Thanks,

  • Hi kalaranjini,

    Welcome to TI e2e community.
    Generally, the error you mentioned occurs if you are not setting the proper partition in the boot args from u-boot. Please check it.
    Also,
    Which is the Soc you are using?
    You have EVM/starter kit or a custom board?
    Which is the kernel version you are trying to boot?
    Are you able to get to the root shell/console after the boot?

    Thanks,
    Prabhuraj
    BlackPepper Technologies