Part Number: AM5728
Tool/software: Linux
Hello
I'm running SDK4.0, 802.1d Ethernet bridging is active in Kernel. Otherwise it's all standard for IDK5728
Setup:
- PC attached to eth0, 192.168.0.3
- PC attached to eth2, 192.168.0.4
- IDK5728
I entered on serial console:
ifconfig eth0 0.0.0.0
ifconfig eth2 0.0.0.0
brctl addbr mybridge
brctl addif mybridge eth0
brctl addif mybridge eth2
ifconfig mybridge up
Test 1 result: Pinging between PCs does not work!
Then I assigned an IP address to the bridge:
ifconfig mybridge down
ifconfig mybridge 192.168.0.20 netmask 255.255.255.0
Test 2 result: Pinging between PCs does not work! However I can ping PCs from Sitara and I can ping bridge address from PC.
What wrong? Is there anything missing in the kernel?
Thanks for help, Chris