Other Parts Discussed in Thread: AM1808
Just how critical is it to meet DQLM and CACLM, the DQS/D and CAC nominal trace length parameters? My current routing exceeds DQLM by 650-700 mils. Fixing this will require rotating the DDR memory 90 degrees counter-clockwise which will require moving a bunch of other stuff. I'm also a bit out on CACLM. However I don’t understand why matching net classes to their max Manhattan length would matter all that much. It should be enough to match net classes within themselves and to their clocks, and keep the max lengths reasonable in comparison to the clock cycle time.
Routing length analysis below:
| Pre-Term | Post-Term | pre length | post length | Total Length | CACLM | Max Delta to CACLM | Actual Delta to CACLM | Max CAC to CAC Skew | Actual CAC to CAC Max Skew | Actual CAC to CAC Min Skew | Max CLKP to CLKN Skew | Actual CLK Skew | |||
| P_DDR_CLKN | M_DDR_CKP | 249.93 | 970.36 | 1220 | 1177 | 50 | 43 | 100 | -53 | 14 | 25 | 14 | |||
| P_DDR_CLKP | M_DDR_CKN | 232.47 | 974.11 | 1207 | 1177 | 50 | 30 | 100 | -66 | 0 | 25 | -14 | |||
| P_DDR_A0 | M_DDR_A0 | 257.33 | 997.09 | 1254 | 1177 | 50 | 77 | 100 | -19 | 48 | |||||
| P_DDR_A1 | M_DDR_A1 | 233.76 | 974.1 | 1208 | 1177 | 50 | 31 | 100 | -65 | 1 | |||||
| P_DDR_A10 | M_DDR_A10 | 245.59 | 979.1 | 1225 | 1177 | 50 | 48 | 100 | -48 | 18 | |||||
| P_DDR_A11 | M_DDR_A11 | 259.18 | 975.37 | 1235 | 1177 | 50 | 58 | 100 | -39 | 28 | |||||
| P_DDR_A12 | M_DDR_A12 | 246.04 | 981.3 | 1227 | 1177 | 50 | 50 | 100 | -46 | 21 | |||||
| P_DDR_A13 | M_DDR_A13 | 236.16 | 998.68 | 1235 | 1177 | 50 | 58 | 100 | -38 | 28 | |||||
| P_DDR_A2 | M_DDR_A2 | 246.58 | 988.31 | 1235 | 1177 | 50 | 58 | 100 | -38 | 28 | |||||
| P_DDR_A3 | M_DDR_A3 | 233.05 | 975.45 | 1209 | 1177 | 50 | 32 | 100 | -65 | 2 | |||||
| P_DDR_A4 | M_DDR_A4 | 238.35 | 986.18 | 1225 | 1177 | 50 | 48 | 100 | -49 | 18 | |||||
| P_DDR_A5 | M_DDR_A5 | 238.5 | 991.65 | 1230 | 1177 | 50 | 53 | 100 | -43 | 24 | |||||
| P_DDR_A6 | M_DDR_A6 | 240.86 | 987.26 | 1228 | 1177 | 50 | 51 | 100 | -45 | 22 | |||||
| P_DDR_A7 | M_DDR_A7 | 233.1 | 978.71 | 1212 | 1177 | 50 | 35 | 100 | -61 | 5 | |||||
| P_DDR_A8 | M_DDR_A8 | 272.77 | 1000.28 | 1273 | 1177 | 50 | 96 | 100 | 0 | 66 | |||||
| P_DDR_A9 | M_DDR_A9 | 240.02 | 986.51 | 1227 | 1177 | 50 | 50 | 100 | -47 | 20 | |||||
| P_DDR_BA0 | M_DDR_BA0 | 232.94 | 998.2 | 1231 | 1177 | 50 | 54 | 100 | -42 | 25 | |||||
| P_DDR_BA1 | M_DDR_BA1 | 278.39 | 991.38 | 1270 | 1177 | 50 | 93 | 100 | -3 | 63 | |||||
| P_DDR_BA2 | M_DDR_BA2 | 243.95 | 985.75 | 1230 | 1177 | 50 | 53 | 100 | -43 | 23 | |||||
| P_DDR_CASN | M_DDR_CASN | 268.14 | 989.13 | 1257 | 1177 | 50 | 80 | 100 | -16 | 51 | |||||
| P_DDR_CKE | M_DDR_CKE | 233.59 | 979.26 | 1213 | 1177 | 50 | 36 | 100 | -60 | 6 | |||||
| P_DDR_CSN | M_DDR_CSN | 267.28 | 1000.24 | 1268 | 1177 | 50 | 91 | 100 | -6 | 61 | |||||
| P_DDR_RASN | M_DDR_RASN | 266.79 | 986.76 | 1254 | 1177 | 50 | 77 | 100 | -20 | 47 | |||||
| P_DDR_WEN | M_DDR_WEN | 235.97 | 989.27 | 1225 | 1177 | 50 | 48 | 100 | -48 | 19 | |||||
| Average | 1233 | ||||||||||||||
| Pre-Term | Post-Term | Pre-Term Length | Post-Term Length | Total Length | DQLM | Max Delta to DQLM | Actual Delta to DQLM | Max D to DQS Skew | Actual D to DQS Skew | Max D to D Skew | Actual D to D Max Skew | Actual D to D Min Skew | Max DQS to DQS Skew | Actual DQS to DQS Skew | |
| M_DDR_D0 | P_DDR_D0 | 255.91 | 1686.63 | 1943 | 1271 | 50 | 672 | 100 | -1 | 100 | 0 | 27 | |||
| M_DDR_D1 | P_DDR_D1 | 251.83 | 1665.6 | 1917 | 1271 | 50 | 646 | 100 | -26 | 100 | -25 | 1 | |||
| M_DDR_D2 | P_DDR_D2 | 264.3 | 1659.1 | 1923 | 1271 | 50 | 652 | 100 | -20 | 100 | -19 | 7 | |||
| M_DDR_D3 | P_DDR_D3 | 258.07 | 1666.33 | 1924 | 1271 | 50 | 653 | 100 | -19 | 100 | -18 | 8 | |||
| M_DDR_D4 | P_DDR_D4 | 259.87 | 1666 | 1926 | 1271 | 50 | 655 | 100 | -18 | 100 | -17 | 10 | |||
| M_DDR_D5 | P_DDR_D5 | 250.5 | 1665.54 | 1916 | 1271 | 50 | 645 | 100 | -28 | 100 | -27 | 0 | |||
| M_DDR_D6 | P_DDR_D6 | 266.06 | 1658.61 | 1925 | 1271 | 50 | 654 | 100 | -19 | 100 | -18 | 9 | |||
| M_DDR_D7 | P_DDR_D7 | 252.55 | 1664.58 | 1917 | 1271 | 50 | 646 | 100 | -27 | 100 | -25 | 1 | |||
| M_DDR_DQM0 | P_DDR_DQM0 | 264.26 | 1665.13 | 1929 | 1271 | 50 | 658 | 100 | -14 | 100 | -13 | 13 | |||
| M_DDR_DQS0 | P_DDR_DQS0 | 263.49 | 1680.24 | 1944 | 1271 | 50 | 673 | 25 | 2 | ||||||
| M_DDR_D8 | P_DDR_D8 | 287.68 | 1672.47 | 1960 | 1271 | 50 | 689 | 100 | 18 | 100 | -14 | 50 | |||
| M_DDR_D9 | P_DDR_D9 | 251.32 | 1663.78 | 1915 | 1271 | 50 | 644 | 100 | -27 | 100 | -59 | 5 | |||
| M_DDR_D10 | P_DDR_D10 | 252.02 | 1674.66 | 1927 | 1271 | 50 | 656 | 100 | -15 | 100 | -47 | 16 | |||
| M_DDR_D11 | P_DDR_D11 | 286.44 | 1687.6 | 1974 | 1271 | 50 | 703 | 100 | 32 | 100 | 0 | 64 | |||
| M_DDR_D12 | P_DDR_D12 | 278.69 | 1662.47 | 1941 | 1271 | 50 | 670 | 100 | -1 | 100 | -33 | 31 | |||
| M_DDR_D13 | P_DDR_D13 | 258.67 | 1679.63 | 1938 | 1271 | 50 | 667 | 100 | -4 | 100 | -36 | 28 | |||
| M_DDR_D14 | P_DDR_D14 | 252.13 | 1658.18 | 1910 | 1271 | 50 | 639 | 100 | -32 | 100 | -64 | 0 | |||
| M_DDR_D15 | P_DDR_D15 | 250.75 | 1663.2 | 1914 | 1271 | 50 | 643 | 100 | -28 | 100 | -60 | 4 | |||
| M_DDR_DQM1 | P_DDR_DQM1 | 291.3 | 1658.96 | 1950 | 1271 | 50 | 679 | 100 | 8 | 100 | -24 | 40 | |||
| M_DDR_DQS1 | P_DDR_DQS1 | 280.55 | 1661.39 | 1942 | 1271 | 50 | 671 | 25 | -2 | ||||||
| Average | 1932 | ||||||||||||||
| Pre-Term1 | Pre-Term2 | Post-Term | Pre-Term1 Length | Pre-Term2 Length | Post-Term Length | Total Length | CKB0B1 | Max Skew to CKB0B1 | Actual Skew to CKB0B1 | ||||||
| P_DDR_DQGATE0 | P_DDR_DQGATE1 | DDR_DQGATE | 1039.14 | 1041.67 | 1036.8 | 3118 | 3156 | 100 | -39 |