This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/EVMK2H: failure to re-enable PSC module on EVMK2H

Genius 13655 points
Part Number: EVMK2H


Tool/software: Linux

Hello Champs,

Customer failed to re-enable all of the PSC modules. 

He used MCSDK 3_00_03_15, there is a function named do_psc_cmd to control the PSC

1. Firest excuting the command psc  15   di in Uboot  to disable the DSP CORE0 module, the emulator can not connect to the DSP0. 

2. Then excuting the command psc  15   en to re-enable the DSP CORE0, but the emulator still can not connect to the DSP0. 

Does the mean the PSC modules could not dynamically enable/disable?

Thanks.

Rgds
Shine