This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359: DDR3 software leveling fails

Part Number: AM3359

Hi all,

My customers use "DDR3_slave_ratio_search_auto.out", they all return with a value of 0, like the console below.

If PHY_INVERT_CLKOUT  = 0, a value other than 0 is returned.

Does anyone know the reason why "DDR3_slave_ratio_search_auto.out" returns 0?

===============Console==========================

[CortxA8]

Enter the PHY_INVERT_CLKOUT value (0 or 1) from the spreadsheet

1

 

Enter the Seed RD_DQS_SLAVE_RATIO Value in Hex to search the RD DQS Ratio Window

40

 

Enter the Seed FIFO_WE_SLAVE_RATIO Value in Hex to search the RD DQS Gate Window

114

 

Enter the Seed WR_DQS_SLAVE_RATIO Write DQS Ratio Value in Hex to search the Write DQS Ratio Window

78

 

***************************************************************

           The Slave Ratio Search Program Values are...

***************************************************************

PARAMETER                       MAX  |  MIN  | OPTIMUM |  RANGE      

***************************************************************

DATA_PHY_RD_DQS_SLAVE_RATIO    0x000 | 0x000 |  0x000  | 0x000

DATA_PHY_FIFO_WE_SLAVE_RATIO   0x000 | 0x000 |  0x000  | 0x000

DATA_PHY_WR_DQS_SLAVE_RATIO    0x000 | 0x000 |  0x000  | 0x000

DATA_PHY_WR_DATA_SLAVE_RATIO   0x000 | 0x000 |  0x000  | 0x000

***************************************************************

rd_dqs_range = 0

fifo_we_range = 0

wr_dqs_range = 0

wr_data_range = 0

 

Optimal values have been found!!

 

***************************************************************

           The Slave Ratio Search Program Values are...

***************************************************************

PARAMETER                       MAX  |  MIN  | OPTIMUM |  RANGE      

***************************************************************

DATA_PHY_RD_DQS_SLAVE_RATIO    0x000 | 0x000 |  0x000  | 0x000

DATA_PHY_FIFO_WE_SLAVE_RATIO   0x000 | 0x000 |  0x000  | 0x000

DATA_PHY_WR_DQS_SLAVE_RATIO    0x000 | 0x000 |  0x000  | 0x000

DATA_PHY_WR_DATA_SLAVE_RATIO   0x000 | 0x000 |  0x000  | 0x000

***************************************************************

Best reagrds,

Sasaki