Other Parts Discussed in Thread: TPS659037, , TPS659039-Q1
Can TPS659037 PMIC be used for DRA756
This is not an automotive application
PMIC need not be Q1 qualified
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can TPS659037 PMIC be used for DRA756
This is not an automotive application
PMIC need not be Q1 qualified
Hello Shreenidhi,
From a device spec perspective, there are only two differences:
1. TPS659037 offers LDO4, TPS659039-Q1 does not.
2. TPS659037 is not automotive qualified, TPS659039-Q1 is.
There are other OTP differences between the available versions of TPS659037 and TPS659039-Q1. TPS6590378ZWSR is the same configuration is O9039A389IZWSRQ1 with the following changes:
1. TPS6590378 uses an external crystal
2. TPS6590378 has a shorter power-down sequence
3. TPS6590378 adds LDO4, so that LDO3 + LDO4 are used to power the PHY domains.
So if your DRA756 application is within the 0x89 capability (DSPEVE + GPU + IVA < 4A), then TPS6590378ZWR should work.
There is a second TPS659037 configuration called TPS6590379ZWSR. This configuration has a separate buck for each core rail, but uses LDO2 to power VDDS18V. So if your application uses < 300mA on VDDS18V, then you could use TPS6590379ZWSR.
Both of these configurations are described in the TPS659037 user's guide. If your current requirements fall within these requirements, TPS659037 should work. If not, then you may need to use TPS659039-Q1.
Regards,
Karl