Tool/software: Starterware
I have two commands in the hwi. One is to read the FPGA parameters through GPMC, and one is to write FPGA parameters, RDCYCLETIME is configured to be 7, WRCYCLETIME is configured to be 7。
test result is:first read commands is 7 clk(70ns),next write commands is 7 clk(70ns)too,but between the two commands have More than 15 clk. why?GPMC issue.docx