This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5726: DDR3 termination question

Part Number: AM5726


I am looking at using some resistor arrays or 0201 parts for the line terminations on the DDR3 memory bus. The parts in question are the resistors on page 23 of the EVM. (TI_AM572XEVM_REV_A3a.PDF schematic)

 

The resistor arrays I am finding are only available in 5% tolerance versus 1% for the 0402 discretes. I am not sure how that would affect performance.

The problem with using 0201 discrete resistors is because the  design guide mentions inductance issues with parts smaller than 0402.

 

And the EVM uses 0402 footprints that are not IPC96 compliant, so we can’t place 0402 parts where they are placed in the EVM design.

We are specing DDR3-1600 (1.25 nS) and DDR3-1866 (1.07 nS) parts but planning to run them at DDR3-1066 (533 MHz) speed. Also the parts will be set to DDR3L voltage levels (1.35V).

 

My question is which issue would cause more problems for the design? Inductance issues with 0201 parts or tolerance issues with the resistor arrays?

  • Can you specify where exactly did you see that "the  design guide mentions inductance issues with parts smaller than 0402"? I couldn't find such a statement.

    As for termination tolerances, see parameter CARS324 in Table 8-12 of the AM572x datasheet SR2.0 Rev. C. This specifies that Rtt must be Zo +/- 5Ohms, which gives 10% tolerance at Zo = 50Ohms. 1% terminations are required only on the DDR_CLK lines (parameter CARS323).
  • Can’t seem to find the document with that information in it now. But the table gives me a lot of confidence in using the resistor arrays, so thanks!!