Other Parts Discussed in Thread: AM4377
Tool/software: Starterware
Hi,
We're debugging Dcan peripherals(AM4377),and have some questions about registers related.
1. I don't understand the the function of bit of CTRL(DCAN_IF1CMD),and the relationship with bit TXRQST_NEWDAT(DCAN_IF1CMD).
2. How can I trigger the transmit of the massage?writes the message number to bits [7:0] of the IF1 command register?or set the bit TXRQST_NEWDAT?
Thanks